Associate
March 26, 2020
Question
STM32MP1-DK2 ethernet stress test crash the board
- March 26, 2020
- 6 replies
- 3306 views
Hello
On a STM32MP1-DK2 discovery board, running the latest starter image, flooding the ethernet interface with SYN packages leads to a reboot of the system. This behavior is reproducible and appears after around 30 secs.
I stress tested the network interface of the STM32MP1-DK2 board with high loads, generated by a self written SYN flood application.
The board is connected via Gbit Ethernet to a developer PC, which sends the SYN packets (around 400Mb/s on sender device).
After around 30 seconds the boards reboots due to a stack exception.
Is this issue already known?
I appended the debug print over the serial interface during the network attack.
Thank you and best regards
Florian