STM32MP1 QSPI Boot problem
Hello everyone,
I'm curently working on a custom STM32MP1 board with a QSPI Nor flash. The NOR Flash seems to work perfectly in Uboot Basic after the modification we have done. The Data are MD5 checked and the SPL is at address 0x0 of the NOR Flash. Evrerything here https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview about the Boot in Nor Flash is respected.
But when we change our BOOT mode Selection, It doesn't boot.
We can only mesure the CS of the NOR FLASH and we see that it is asserted once quickly shortly after reset. But that's all.
My question is: Do you support only some NOR FLASH by reading the JEDEC number in ROM Code ?
Best Regards,
Anthony Harivel