STM32MP135F QT5 can't execute gui aplication
Hi,
I have a relatively easy question for the OpenStLinux I guess.
I have a correctly prepared sdk image with QT (bitbake -k st-example-image-qt and bitbake -k st-example-image-qt -c populate_sdk) but can't correctly configure weston. I have a similar configuration to the official STM32MP135DK2 with a slight difference, 24 RGB interface. My display working correctly, I can see wallpaper and play mp4, so the driver and system are configured correctly.
When I try to execute my application I get something like
QStandardPaths: XDG_RUNTIME_DIR not set, defaulting to '/tmp/runtime-root'
[ 1] Failed to open device: No such file or directory, Try again...
[ 2] Failed to open device: No such file or directory, Try again...
[ 3] Failed to open device: No such file or directory, Try again...
[ 4] Failed to open device: No such file or directory, Try again...
[ 5] _OpenDevice(1093): FATAL: Failed to open device, errno=No such file or directory.
[ 6] Failed to open device: No such file or directory, Try again...
[ 7] Failed to open device: No such file or directory, Try again...
[ 8] Failed to open device: No such file or directory, Try again...
[ 9] Failed to open device: No such file or directory, Try again...
[ 10] _OpenDevice(1093): FATAL: Failed to open device, errno=No such file or directory.
The problem is that the above info doesn't indicate what device can't be opened.
What do I need to add to my meta-layer to be able to execute the qt5 application?
Thanks for any hints
BR Michal