stm32mp15 JTAG on m4 core with yocto5: optee permission failure
Hi everyone,
I'm working on a custom board based on STM32MP157F-DK2. I am running Yocto 5.0.3 (scarthgap) with trusted boot (not signed).
I could build the Zephyr (3.7.0) rpmsg sample that worked out of the box:
https://docs.zephyrproject.org/latest/samples/subsys/ipc/openamp_rsc_table/README.html
Now the issue is when I tried to debug the m4 core with a JTAG, the board crashes, here is what I see on the Linux console:
E/TC:0 tzc_it_handler:79 TZC permission failure
E/TC:0 dump_fail_filter:420 Permission violation on filter 0
E/TC:0 dump_fail_filter:425 Violation @0xdeadbef0, non-secure privileged read, AXI ID 1
E/TC:0 Panic at core/arch/arm/plat-stm32mp1/plat_tzc400.c:84 <tzc_it_handler>
E/TC:0 TEE load address @ 0xde000000
E/TC:0 Call stack:
E/TC:0 0xde002961
E/TC:0 0xde017cd1
E/TC:0 0xde0046d7
E/TC:0 0xde0179f7
E/TC:0 0xde023679
E/TC:0 0xde000348
I started JLinkGDBServer with those parameters:
JLinkGDBServer -port 2331 -s -device STM32MP15XX_M4 -endian little -speed 4000 -vd -nohalt -noreset
I can see however that the debugger has a lot of errors while reading some CPU registers or memory area:
Read register 'r0' (4 bytes) from hardware: 0xEFBEADDE
ERROR: Cannot read register 1 (R1) while CPU is running
// ...
Read register 'pc' (4 bytes) from hardware: 0xEFBEADDE
ERROR: Cannot read register 16 (XPSR) while CPU is running
Read register 'xpsr' (4 bytes) from hardware: 0xEFBEADDE
Read 4 bytes @ address 0xDEADBEEE (Data = 0x00002300)
Downloading 664 bytes @ address 0x00000000 - Verified OK
Downloading 16136 bytes @ address 0x00000298 - Verify failed (expected 0x61 read 0xFFFFFFF0 @ 0x00002299)
Downloading 11412 bytes @ address 0x000041A0 - Verify failed (expected 0x30 read 0x00 @ 0x000061A0)
Downloading 8 bytes @ address 0x00006E34 - Verify failed (expected 0xFFFFFF94 read 0xFFFFFFAA @ 0x00006E34)
Downloading 176 bytes @ address 0x00006E3C - Verified OK
Downloading 320 bytes @ address 0x00006EEC - Verified OK
Downloading 1200 bytes @ address 0x0000702C - Verified OK
Downloading 1384 bytes @ address 0x000074DC - Verify failed (expected 0x45 read 0xFFFFFFAA @ 0x000074DC)
Downloading 136 bytes @ address 0x00007A44 - Verify failed (expected 0x00 read 0xFFFFFFAA @ 0x00007A44)
// ...
ERROR: Cannot read register 15 (R15) while CPU is running
Writing register 'pc' = 0x000011D4
Writing register 'xpsr' = 0xDFADBEEF
Starting target CPU...
Is there something that I'm missing in optee/ATF to allow JTAG debugging? Any pointers on the fine wiki?
Thanks and all the best!
Guy