Hi,
the pin 41 of KSZ9031 should provide the 125 MHz clock to STM32MP1 (and this is the simpler and preferred solution), but in your schematic it is instead connected only to a test point.
If you cannot rework your board, you need to provide the 125 MHz internally in STM32MP1.
Check the STM32MP1 Reference Manual at chapter 10.4.8 "clock distribution for Ethernet (ETH)".
The input named "ETH_CLK125" is the one missing in your board, so has to be replaced with a 125 MHz clock arriving from pll4_p_ck or pll3_q_ck. Now we need to set all the internal switches to achieve this.
Use also the document Documentation/devicetree/bindings/net/stm32-dwmac.txt for reference.
1) mux between ETH_CLK125 and eth_clk_fb: change its position adding DT property:
st,eth_clk_sel = <1>;
2) enable the gate controlled by ETHCKEN: for this you need to add two more clocks in the DT:
To clock-names add "eth-ck" and "syscfg-clk"
To clocks add ETHCK_K and SYSCFG
The point 1) and 2) can be put in your board DT as:
ðernet0 {
status = "okay";
st,eth_clk_sel = <1>;
clock-names = "stmmaceth",
"mac-clk-tx",
"mac-clk-rx",
"eth-ck",
"syscfg-clk",
"ethstp";
clocks = <&rcc ETHMAC>,
<&rcc ETHTX>,
<&rcc ETHRX>,
<&rcc ETHCK_K>,
<&rcc SYSCFG>,
<&rcc ETHSTP>;
};
Now it remains the mux between pll4_p_ck or pll3_q_ck and the frequency from the PLL. This has to be done in the DT of tf-a (if you use secure boot) or DT of U-Boot (if you use the basic boot). The DT is the same in the two cases, just stored in a different file:
- tf-a has DT in folder ./fdts/
- u-boot has DT in folder ./arch/arm/dts/
At linux boot, this command gives you the dump of the clock tree. You need to verify there if the clock frequency is correct
cat /sys/kernel/debug/clk/clk_summary
You also need to set a frequency that is suitable for all the users of the same PLL
Let's go to edit the DT!
4) mux source: replace CLK_ETH_DISABLED with CLK_ETH_PLL4P or with CLK_ETH_PLL3Q
in my test I used pll4_p
5) change the numbers in node "pll3: st,pll@2" or "pll4: st,pll@3"
one possible settings for pll4_p at 125 MHz (suppose crystal on HSE is 24 MHz) is
/* VCO = 750.0 MHz, P=125, Q=62.5, R=62.5 */
pll4: st,pll@3 {
cfg = <3 124 5 11 11 PQR(1,1,1)>;
};