Skip to main content
debugging
Lead
May 8, 2025
Question

STM32MP2 ECO 6 USB Gadget STM32MP257F-DK board locks up and freezes

  • May 8, 2025
  • 0 replies
  • 299 views

stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06.tar-gz from ECO 6.0 and only enabling the USB gadget drivers in .config, rebuilding the kernel and modules

The board freezes :

1. When the gadget driver  is loaded and USB cable to host is plugged in

2. When the gadget driver is loaded w/o USB cable plugged in, the gadget is loaded and board does not freezen When plugging in the USB cable to the host, the board freezes.

Another vendor's 64 bit ARM board with kernel 6.6.xx does not freeze. Is there anything to debug with the device tree or otherwise to find the reason for lock up ?