STM32MP2 OP-TEE RISAF access permissions
Hi,
I am debugging the STM32MP257F-EV1 board via a JTAG debugger . The kernel version is 6.1.82.
I have a sample application that runs on Linux and I am trying to debug it.
When I set a breakpoint in the application, I get the following message on the Kernel prompt:
---------------------------------------------------------------------
E/TC:0 stm32_iac_itr:192 IAC exceptions [159:128]: 0x200
E/TC:0 stm32_iac_itr:197 IAC exception ID: 137
E/TC:0 stm32_risaf_dump_erroneous_data:256
DUMPING DATA FOR risaf@420d0000
E/TC:0 stm32_risaf_dump_erroneous_data:257 =====================================================
E/TC:0 stm32_risaf_dump_erroneous_data:258 Status register (IAESR0): 0xb1
E/TC:0 stm32_risaf_dump_erroneous_data:266 -----------------------------------------------------
E/TC:0 stm32_risaf_dump_erroneous_data:268 Faulty address (IADDR0): 0x10b4dc8dc
E/TC:0 stm32_risaf_dump_erroneous_data:287 =====================================================
E/TC:0 Panic at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/drivers/firewall/stm32_iac.c:212 <stm32_iac_itr>
E/TC:0 TEE load address @ 0x82000000
E/TC:0 Call stack:
E/TC:0 0x82007efc
E/TC:0 0x82041b80
E/TC:0 0x8202c2fc
E/TC:0 0x8203f6b4
E/TC:0 0x82013d30
E/TC:0 0x820017dc
I/TC: Halting CPU 1
---------------------------------------------------------------------
I think this is related to the firewall and RIF(Resource Isolation Framework).
The prints explain that there has been an access violation at address 0x10b4dc8dc in the RISAF (Resource Isolation Slave unit for Address space protection) device at index 137.
On searching the CPU Reference manual, it was found that #137 pertains to [RISAF4 (DDR-SDRAM)].
In the OP-TEE source code, it was found that access has been enabled in the below DTS files:
1. [~\core\arch\arm\dts\stm32mp257f-ev1-ca35tdcid-resmem.dtsi]
linuxkernel2: linuxkernel2@100000000 {
reg = <0x1 0x00000000 0x0 0x80000000>;
no-map;
};
2. [~\core\arch\arm\dts\stm32mp257f-ev1-ca35tdcid-rif.dtsi]
&linuxkernel2 {
st,protreg = <RISAFPROT(RISAF_REG_ID(15), RIF_CID0_BF|RIF_CID1_BF, RIF_CID0_BF|RIF_CID1_BF, RIF_UNUSED, RIF_NSEC, RIF_ENC_DIS, RIF_BREN_EN)>;
};
&risaf4 {
memory-region= <&tfm_code>, <&cm33_cube_fw>, <&tfm_data>, <&cm33_cube_data>, <&ipc_shmem>, <&spare1>, <&bl31_context>, <&op_tee>, <&linuxkernel1>, <&gpu_reserved>, <<dc_sec_layer>, <<dc_sec_rotation>, <&linuxkernel2>;
};
I think if access is granted or disabled, then a breakpoint can be set.
Is it possible to disable the OP-TEE firewall monitoring for DDR-SDRAM area?
I would appreciate any help. Thank you.