Solved
stm32mp255 USB-C VBUS GPIO device tree configuration
I am trying to configure a USB-C connector on a peripheral device to detect VBUS via GPIO (PH9). I have tried several iterations using the following device tree documentation.
The only way I have been able to get USB traffic to occur is by using the role-switch-default-mode attribute, but that comes with the warning about VBUS:
Forcing default mode bypasses the vbus detection, which is normally required to raise the pull-up resistor on D+ data line. This makes it non compliant with USB specifications. Recommended method to implement peripheral only role, is to use GPIO to detect Vbus,
And I suspect this warning is the reason why USB traffic doesn't come back after coming back out of suspend/low-power mode.
Example snippet of a configuration I've tried is as follows:
/ {
usb_c_connector {
compatible = "usb-c-connector";
label = "USB-C Connector";
type = "usb-c";
vbus-gpios = <&gpioh 9 (GPIO_ACTIVE_HIGH | GPIO_PULL_UP)>;
vbus-supply = <&scmi_vdd3v3_usb>;
port {
dwc3_ep: endpoint {
remote-endpoint = <&typec_ep>;
};
};
};
};
&usb3dr {
status = "okay";
dwc3:usb@48300000{
maximum-speed = "high-speed";
usb-role-switch;
port {
typec_ep: endpoint {
remote-endpoint = <&dwc3_ep>;
};
};
};
};Is there an example using the DWC3 driver with a `typec` connector and/or VBUS via GPIO?