STM32MP257 - Unable to handle kernel paging request at virtual address dead000000000108
Hi,
I have few custom boards with STM32MP257 mostly running PTP related tasks. Once in a while (once in a few days of continuous run) I have noticed the following error in the dmesg (as it seems UART related - I have 4 UARTs enabled in the DT, while 3 of them have DMA enabled (the console one does not have the DMA enabled), but only one UART (other than console) is being used in the system for RX only):
[251158.390476] Unable to handle kernel paging request at virtual address dead000000000108
[251158.392934] Mem abort info:
[251158.395854] ESR = 0x0000000096000044
[251158.399679] EC = 0x25: DABT (current EL), IL = 32 bits
[251158.405114] SET = 0, FnV = 0
[251158.408235] EA = 0, S1PTW = 0
[251158.411457] FSC = 0x04: level 0 translation fault
[251158.416489] Data abort info:
[251158.419408] ISV = 0, ISS = 0x00000044, ISS2 = 0x00000000
[251158.425041] CM = 0, WnR = 1, TnD = 0, TagAccess = 0
[251158.430173] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0
[251158.435607] [dead000000000108] address between user and kernel address ranges
[251158.442949] Internal error: Oops: 0000000096000044 [#1] PREEMPT SMP
[251158.449289] Modules linked in: marvell cfg80211 rfkill usb_f_ncm u_ether libcomposite spidev crct10dif_ce phy_stm32_usb2phy rtc_stm32 mr75203 hantro_vpu v4l2_jpeg v4l2_vp9 v4l2_h264 v4l2_mem2mem videobuf2_dma_contig videobuf2_memops videobuf2_v4l2 videodev at24 videobuf2_common mc stm32_cryp dwc3_stm32 stm32_lptimer crypto_engine spi_stm32 libdes stm32_crc32 stm32_timers mailbox_client_cdev stm32_m0_rproc stm32_rproc irq_rpmsg sch_fq_codel nfnetlink ip_tables ipv6
[251158.490832] CPU: 0 PID: 243312 Comm: kworker/0:2 Not tainted 6.6.78-gaf978724e078-dirty #1
[251158.499183] Hardware name: STMicroelectronics STM32MP257F CARD (DT)
[251158.505923] Workqueue: pm pm_runtime_work
[251158.510064] pstate: 200000c5 (nzCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[251158.517110] pc : vchan_tx_submit+0x58/0xd0
[251158.521343] lr : vchan_tx_submit+0x28/0xd0
[251158.525574] sp : ffff8000828cbba0
[251158.528997] x29: ffff8000828cbba0 x28: 0000000000000000 x27: 0000000000000000
[251158.536250] x26: ffff0000040fdcf4 x25: 0000000000000000 x24: 0000000000000000
[251158.543502] x23: 0000000000000000 x22: ffff000006d5c780 x21: ffff00000494a6a0
[251158.550754] x20: 000000000003d505 x19: ffff0000064823c0 x18: 0000000000000000
[251158.558006] x17: ffff7fffb5e89000 x16: ffff800080000000 x15: 001015373f0be4e6
[251158.565259] x14: 0000000000000001 x13: 0000000000000001 x12: 0000000000000001
[251158.572510] x11: 0000000000000000 x10: 0000000000000003 x9 : 0000000000000000
[251158.579762] x8 : ffff00000494a748 x7 : 0000000000084000 x6 : 0000000000000800
[251158.587014] x5 : ffff00000494a758 x4 : dead000000000100 x3 : dead000000000122
[251158.594266] x2 : ffff000006482438 x1 : 0000000000000000 x0 : ffff00000494a740
[251158.601518] Call trace:
[251158.604038] vchan_tx_submit+0x58/0xd0
[251158.607968] stm32_usart_rx_dma_start_or_resume+0xd8/0x234
[251158.613509] stm32_usart_runtime_resume+0x78/0xe8
[251158.618344] pm_generic_runtime_resume+0x2c/0x44
[251158.623081] __genpd_runtime_resume+0x30/0x80
[251158.627517] genpd_runtime_resume+0x114/0x29c
[251158.631954] __rpm_callback+0x48/0x1d8
[251158.635788] rpm_callback+0x6c/0x78
[251158.639420] rpm_resume+0x490/0x6b4
[251158.642952] pm_runtime_work+0x84/0xc8
[251158.646882] process_one_work+0x144/0x29c
[251158.650917] worker_thread+0x324/0x43c
[251158.654848] kthread+0x110/0x114
[251158.658077] ret_from_fork+0x10/0x20
[251158.661813] Code: 1a9fc694 b9001074 b8078454 a9478e64 (f9000483)
[251158.668051] ---[ end trace 0000000000000000 ]---
[251158.672781] note: kworker/0:2[243312] exited with irqs disabled
[251158.679385] note: kworker/0:2[243312] exited with preempt_count 1
after this event, the system begins acting strangely - the heartbeat led blinking much faster than usual (although top command does not seem to show high CPU load, some services cannot be stopped - like I can run journalctl of some process, but I cannot stop it, the process just getting hang and kill does not help.
Any ideas of what can cause it?
Thanks!
Alexey.