Skip to main content
Associate III
August 31, 2024
Question

USB 2nd Port detection in uboot

  • August 31, 2024
  • 0 replies
  • 639 views
Hello
 
We are Working on a custom board with STM32MP157AAA3 processor.We are using Buildroot(V2023.08.2) for checking USB 2nd Port in which the PHY port 2 is configured as host controller using UTMI .
 
we referred the below link to configure the dts :
 
We are configuring the USB in dts file exactly the same in Uboot (V2023.10) and Linux(V5.13), It works in Linux but not in Uboot 
 
We are attaching the configuration of our dts file below.Hope you could Verify it and suggest us where we are going wrong.
 
 
Aks_1-1725081193695.png

 

Thanks & Regards
Akshitha Pattem