which gcc version for openstlinux STM32MP1 native compilation?
I tried to add development tools to my openSTLinux using apt-get install, but couldn't find gcc.
so I tried to create a distribution including gcc, make, cmake and git.
When I search for available recipes for gcc using
find ../layers/ -iname "*gcc*.bb"
I get the following list of gcc tools
../layers/meta-st/meta-st-stm32mp/recipes-devtools/gcc-arm-none-eabi/gcc-arm-none-eabi-native_11.bb
../layers/meta-st/meta-st-stm32mp/recipes-devtools/gcc-arm-none-eabi/nativesdk-gcc-arm-none-eabi_11.bb
../layers/openembedded-core/meta/recipes-devtools/gcc/gcc-cross-canadian_12.2.bb
../layers/openembedded-core/meta/recipes-devtools/gcc/libgcc-initial_12.2.bb
../layers/openembedded-core/meta/recipes-devtools/gcc/gcc-cross_12.2.bb
../layers/openembedded-core/meta/recipes-devtools/gcc/gcc-crosssdk_12.2.bb
../layers/openembedded-core/meta/recipes-devtools/gcc/gcc-sanitizers_12.2.bb
../layers/openembedded-core/meta/recipes-devtools/gcc/gcc_12.2.bb
../layers/openembedded-core/meta/recipes-devtools/gcc/libgcc_12.2.bb
../layers/openembedded-core/meta/recipes-devtools/gcc/gcc-source_12.2.bb
../layers/openembedded-core/meta/recipes-devtools/gcc/gcc-runtime_12.2.bb
which one should I include in my distribution?
when I try to add "gcc-arm-none-eabi-native" or "nativesdk-gcc-arm-none-eabi" or "libgcc-initial" to the distribution by adding them to the recipe st-image-weston.bb
using
CORE_IMAGE_EXTRA_INSTALL += " gcc-arm-none-eabi-native nativesdk-gcc-arm-none-eabi libgcc-initial"
I get error
ERROR: Task do_populate_sdk in /.../Distribution-Package/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb rdepends upon non-existent task do_package_write_deb in .../Distribution-Package/layers/openembedded-core/meta/recipes-devtools/gcc/libgcc-initial_12.2.bb
and same error for other two recipes
even though I can find the stm-st-stm32mp layer when I rung bitbake-layers show-layers as shown below
stm-st-stm32mp /.../Distribution-Package/layers/meta-st/meta-st-stm32mp 6
core /.../Distribution-Package/layers/openembedded-core/meta 5
Why I am getting this error and how to overcome it?
When I add other gcc recipes to the distribution image and flash it to board, I can't find gcc among installed apps on the board
How can I solve this problem?