Skip to main content
Visitor II
October 24, 2024
Question

2 Host and 1 device USB

  • October 24, 2024
  • 1 reply
  • 689 views

My current application uses 2 USB ports, both connected to USBPHYC (STM32MP157F). The OTG one is used for programming using CubeProgrammer.

My new revision requires 3 USB ports, 2 host and the programming port.

According to https://community.st.com/t5/stm32-mpus-software-development/how-to-enable-3-usb-ports-on-stm32mp1/td-p/269938 it is (still) not possible to configure this in CubeMX.

Im wondering if this configuration is going to work:

USBH_HS1->USBPHYC-> USB_DM/DP1 pins (Host)

USBH_HS2->USBPHYC-> USB_DM/DP2 pins (Host)

USB_OTG->OTG FS Phy->PA11/PA12 pins (device/programming)

AN5031 states that the internal bootROM will use high-speed, which means my suggested setup is not possible?

 

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    October 25, 2024

    Hi @allard 

    yes, what listed in AN5031 will work (although not usual, I know some customers use that).

    You should manually adapt the Device Tree to this case.

    For the flashing, you should also build a specific uBoot (used only for flashing, i.e. only for the part #3 fip-boot line in flashlayout file) which must use USB_DM/DP2 pins as USB_OTG device mode high-speed (so specific Device Tree for this uBoot, like this). Then the flashed uBoot use your 3 port scheme as you need.

    Obviously, you also need a non-standard USB Type-A <-> Type-A cable to connect to the PC to the right board connector (ok as only for production flashload).

     

    Obviously, adding a hub IC as on STM32MP157F-DK is more straightforward (and bring OTG in high-speed), but more external components required.

    Regards.