Skip to main content
Graduate
April 4, 2025
Solved

About choosing memory of STM32MP157

  • April 4, 2025
  • 1 reply
  • 522 views

Hello.

I am designing a circuit with stm32mp157f.

I'm looking for eMMC when choosing memory because 4Gbit slc nand flash is too expensive.

In the datasheet, I read in the data sheet that stm32 supports emmc.

Younjun_0-1743747803589.png

The question is as follows.

  • Is it correct that eMMC can be used even if it is not SLC(pSLC, MLC...) like IS21EF04GP-JCLI-TR?
    (It's my first time using mpu and memory. So it's very difficult for me to choose memory.)

  • Is the QSPI flash of STM32MP157F-ev1 used for RAM?
     
    Younjun_1-1743749091451.png

     

Regards,

Youngjun.

    This topic has been closed for replies.
    Best answer by PatrickF

    Hi @Younjun 

     

    1st question answered in https://community.st.com/t5/stm32-mpus-products/can-i-use-any-kind-of-emmc-for-stm32mp1/td-p/790740

    2nd question answer is No. QUADSPI of STM32MP1 only support Flash.

    RAM is DDR connected on DDRCTRL/DDRPHY (external DDR is mandatory to use the platform as internal RAMs are very small)

    Regards,

    1 reply

    PatrickFAnswer
    Technical Moderator
    April 7, 2025

    Hi @Younjun 

     

    1st question answered in https://community.st.com/t5/stm32-mpus-products/can-i-use-any-kind-of-emmc-for-stm32mp1/td-p/790740

    2nd question answer is No. QUADSPI of STM32MP1 only support Flash.

    RAM is DDR connected on DDRCTRL/DDRPHY (external DDR is mandatory to use the platform as internal RAMs are very small)

    Regards,