Skip to main content
Visitor II
December 7, 2022
Solved

About "VREF+" pin

  • December 7, 2022
  • 4 replies
  • 2790 views

Hi team,

I am developing our PCB referring to the "STM32MP157 EVAL"(MB1263-C04 Board schematic).

https://www.st.com/en/evaluation-tools/stm32mp157f-ev1.html#cad-resources

In the datasheet, VREF+ looks like a voltage output pin, but why is power supply connected to VREF+ in STM32MP157 EVAL?

Best regard,

    This topic has been closed for replies.
    Best answer by QSHAO.1

    in datasheet, it's mentioned that "An external voltage reference can be provided through the VREF+ pin when the internal voltage reference buffer is off". so external Vref+ mode is used on the board.

    4 replies

    Graduate II
    December 7, 2022

    Maybe read the text in the image you posted?

    QSHAO.1Answer
    ST Employee
    December 7, 2022

    in datasheet, it's mentioned that "An external voltage reference can be provided through the VREF+ pin when the internal voltage reference buffer is off". so external Vref+ mode is used on the board.

    ST Employee
    December 7, 2022

    Don't forget to add a 1uF capacitor for decoupling when used as output.

    Technical Moderator
    December 8, 2022

    In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'