Skip to main content
Graduate
January 31, 2025
Question

ADC DMA on stm32mp257 interrupt not triggering

  • January 31, 2025
  • 0 replies
  • 715 views

Hello,

I am trying to get my ADC using DMA working in my freertos program running on the M33 core of the stm32mp257 processor. I set up ADC1 on HPDMA3 using cube MX see config below.

nielsenni101_0-1738352115447.png

I am getting a few issues.

1. If I used the generated code I get a runtime crash because the HAL layer was trying to access of null object hacd->DMA_Handle. I got around that issue by adding this line to HAL_ADC_MspInit()

 

 

 

 

hadc->DMA_Handle = &handle_HPDMA3_Channel11;

 

 

 

 

Not sure why this was not getting generated by MX.

 

2. I was getting another crash because of another reference to null variable pQueueLinkList. MX generated this in HAL_ADC_MspInit(). pQueueLinkList was defined but never initialized to anything. I needed to remove this piece of code as well.

 

 

 

 

if (HAL_DMAEx_List_SetCircularMode(&pQueueLinkList_HPDMACH11) != HAL_OK)
{
 Error_Handler();
}

 

 

 

 

 

Once I got past these issues I was able to start up my program without crashing. Now the main issue that I would like help with is that I do not get the interrupt triggered for HAL_ADC_ConvCpltCallback(). I am calling HAL_ADC_Start_DMA() and HAL_ADC_Stop_DMA().

I do get the interrupt when I call the non DMA versions. HAL_ADC_Start_IT() and HAL_ADC_Stop_IT(). So it seems to be an issue with the DMA.

 

Any ideas? Thanks.

 

Edit: I attached the stm32mp2xx_hal_msp.c and noticed that it is generating stuff for linked list when I have my DMA channel set to standard request mode. Is that what is supposed to be generated?

    This topic has been closed for replies.