Automated unit testing for Yocto builds
Hi!
Is there a way to run unit tests automatically on the STM32MP157-DK2 board? I've managed to flash the device using the STM32 Programmer CLI, but after flashing, I need to manually switch the bootmode to boot from the SD-card.
It would be great if the flash and boot could be triggered completely automatically, e.g. by a Jenkins script. If the device could flash and boot without any manual steps, it would make it possible to run various test scripts completely automatically on the real hardware. Is this in any way possible?