Boot a custom board with STM32MP153CAA from SDMMC2 interface
We have a custom board with and STM32MP153CAA processor and are trying to get it to boot from an SMCC card on SDMMC2 interface. If I loaded the tf and fip files via a UART I am able to get u-boot running and then use the "run bootcmd_mmc0" to boot the linux kernel from the SDMMC2 car from there. So I know that the electrical connection to the SD card is correct. However we'd like to have the whole boot process read from the card at power up.
I have an SD card laid out with the partition scheme used to boot the discovery boards from SDMMC1 and have written the boot loaders to the card. I have tried setting the OTP word 3 to 0x10 which from ST's documentation I would believe should set up the boot from the SDMMC2 card and have set the boot pins to 101 binary which should tell the processor that the primary boot should be from SDMMC card, but if will not boot. I get nothing at all output to UART-4 which I have set up as console nor any indication that the board is trying to read from SDMMC2.
Does anyone have any guidance.