Boot issue in STM32MP257F-DK board
Move from MCU forums: STM32MP25 are MPUs - not MCUs
Hello Experts,
I am using STM32MP257F-DK board and trying to bring up the board with starter package.
I followed the steps as mentioned in this link - https://wiki.st.com/stm32mpu/wiki/STM32MP25_Discovery_kits_-_Starter_Package
The starter package that I have downloaded and flashed - en.FLASH-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06.tar.gz
I was able to flash the SD card successfully as mentioned in section 6.
(Note that I have taken care of boot switches accordingly)
However, when I restart the board for booting, seems there are issues and does not stop at login prompt. Instead stops or boots in loop. Attaching 2 logs with 2 instances of reset. Kindly help to review and suggest work around if have missed any steps.
~R