Resolved the issue.
There was a difference in the .dts file from for the STM32MP25-EV1 board and my custom board with the pin layout for the sdmmc. The evaluation board had this :
&sdmmc2 {
pinctrl-names = "default";
pinctrl-0 = <&sdmmc2_b4_pins_a &sdmmc2_d47_pins_a>;
non-removable;
no-sd;
no-sdio;
st,neg-edge;
bus-width = <8>;
vmmc-supply = <&vdd_emmc>;
vqmmc-supply = <&vddio2>;
status = "okay";
};
/omit-if-no-ref/
sdmmc2_b4_pins_a: sdmmc2-b4-0 {
pins1 {
pinmux = <STM32_PINMUX('E', 13, AF12)>, /* SDMMC2_D0 */
<STM32_PINMUX('E', 11, AF12)>, /* SDMMC2_D1 */
<STM32_PINMUX('E', 8, AF12)>, /* SDMMC2_D2 */
<STM32_PINMUX('E', 12, AF12)>, /* SDMMC2_D3 */
<STM32_PINMUX('E', 15, AF12)>; /* SDMMC2_CMD */
slew-rate = <1>;
drive-push-pull;
bias-pull-up;
};
pins2 {
pinmux = <STM32_PINMUX('E', 14, AF12)>; /* SDMMC2_CK */
slew-rate = <2>;
drive-push-pull;
bias-pull-up;
};
};
/omit-if-no-ref/
sdmmc2_d47_pins_a: sdmmc2-d47-0 {
pins {
pinmux = <STM32_PINMUX('E', 10, AF12)>, /* SDMMC2_D4 */
<STM32_PINMUX('E', 9, AF12)>, /* SDMMC2_D5 */
<STM32_PINMUX('E', 6, AF12)>, /* SDMMC2_D6 */
<STM32_PINMUX('E', 7, AF12)>; /* SDMMC2_D7 */
slew-rate = <1>;
drive-push-pull;
bias-pull-up;
};
};
and I had this :
&sdmmc1 {
pinctrl-names = "default";
pinctrl-0 = <&sdmmc1_pins_mx>;
status = "okay";
/* USER CODE BEGIN sdmmc1 */
non-removable;
no-sd;
no-sdio;
st,neg-edge;
bus-width = <8>;
vmmc-supply = <&vdd_emmc>;
vqmmc-supply = <&vddio2>;
/* USER CODE END sdmmc1 */
};
sdmmc1_pins_mx: sdmmc1_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('D', 8, AF11)>, /* SDMMC1_D7 */
<STM32_PINMUX('D', 9, AF11)>, /* SDMMC1_D6 */
<STM32_PINMUX('D', 10, AF11)>, /* SDMMC1_D5 */
<STM32_PINMUX('D', 11, AF11)>, /* SDMMC1_D4 */
<STM32_PINMUX('E', 0, AF10)>, /* SDMMC1_D2 */
<STM32_PINMUX('E', 1, AF10)>, /* SDMMC1_D3 */
<STM32_PINMUX('E', 2, AF10)>, /* SDMMC1_CMD */
<STM32_PINMUX('E', 4, AF10)>, /* SDMMC1_D0 */
<STM32_PINMUX('E', 5, AF10)>; /* SDMMC1_D1 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 3, AF10)>; /* SDMMC1_CK */
bias-disable;
drive-push-pull;
slew-rate = <3>;
We had to split the pins into two banks like the EV board does. Once we did that we booted fine from emmc. Not sure why that made it work though.