Skip to main content
Visitor II
November 25, 2020
Solved

Build image linux-stm32mp-5.4.56-r0

  • November 25, 2020
  • 2 replies
  • 1428 views

Hello totgehet,

i wanted to build a Kernelmodule for my Projekt so i started to install the SDK and wrote a simple Programm to see if i can make a Programm in the userspace. This works fine. My next step was to Building and deploying the Linux kernel. For that I followed the installation https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package. But when I want to Compile and install on a build directory I get this error from the makefil:

make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040 O="$PWD/../build"

make[1]: Entering directory '/opt/st/stm32mp1/3.1-openstlinux-5.4-dunfell-mp1-20-11-12/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/build'

 GEN    Makefile

scripts/kconfig/conf --syncconfig Kconfig

 GEN    Makefile

 SYSHDR arch/arm/include/generated/uapi/asm/unistd-common.h

 SYSHDR arch/arm/include/generated/uapi/asm/unistd-oabi.h

 SYSHDR arch/arm/include/generated/uapi/asm/unistd-eabi.h

 HOSTCC scripts/dtc/dtc.o

 HOSTCC scripts/dtc/flattree.o

 HOSTCC scripts/dtc/fstree.o

 HOSTCC scripts/dtc/data.o

 HOSTCC scripts/dtc/livetree.o

 HOSTCC scripts/dtc/treesource.o

 HOSTCC scripts/dtc/srcpos.o

 HOSTCC scripts/dtc/checks.o

 HOSTCC scripts/dtc/util.o

 LEX     scripts/dtc/dtc-lexer.lex.c

 YACC   scripts/dtc/dtc-parser.tab.[ch]

 HOSTCC scripts/dtc/dtc-lexer.lex.o

 HOSTCC scripts/dtc/dtc-parser.tab.o

 HOSTCC scripts/dtc/yamltree.o

 HOSTLD scripts/dtc/dtc

 HOSTCC scripts/genksyms/genksyms.o

 YACC   scripts/genksyms/parse.tab.[ch]

 HOSTCC scripts/genksyms/parse.tab.o

 LEX    scripts/genksyms/lex.lex.c

 HOSTCC scripts/genksyms/lex.lex.o

 HOSTLD scripts/genksyms/genksyms

 HOSTCC scripts/kallsyms

 HOSTCC scripts/conmakehash

 HOSTCC scripts/sortextable

 HOSTCC scripts/asn1_compiler

 HOSTCC scripts/sign-file

/opt/st/stm32mp1/3.1-openstlinux-5.4-dunfell-mp1-20-11-12/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/linux-5.4.56/scripts/sign-file.c:25:10: fatal error: openssl/opensslv.h: No such file or directory

  25 | #include <openssl/opensslv.h>

     |         ^~~~~~~~~~~~~~~~~~~~

compilation terminated.

make[2]: *** [scripts/Makefile.host:107: scripts/sign-file] Error 1

make[1]: *** [/opt/st/stm32mp1/3.1-openstlinux-5.4-dunfell-mp1-20-11-12/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/linux-5.4.56/Makefile:1100: scripts] Error 2

make[1]: Leaving directory '/opt/st/stm32mp1/3.1-openstlinux-5.4-dunfell-mp1-20-11-12/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/build'

I checked my SDK and I saw that the Headerfile is available. This is why I have no idea how to fix the build. I hope someone can help me Thanks so far.

    This topic has been closed for replies.
    Best answer by JYune

    It seems like you need OpenSSL development package on your PC. Try this:

    $ sudo apt-get install libssl-dev

    2 replies

    JYuneAnswer
    Visitor II
    November 25, 2020

    It seems like you need OpenSSL development package on your PC. Try this:

    $ sudo apt-get install libssl-dev

    SAman.1Author
    Visitor II
    November 25, 2020

    Thanks now its working i already compiled a simple kernel module.

    Technical Moderator
    November 25, 2020

    Hi @SAman.1​ ,

    Thanks @JYune​ you are right

    To be complete pay attention to install all extra package as per listed here :

    https://wiki.st.com/stm32mpu/wiki/PC_prerequisites#Install_extra_packages

    Olivier