Can I install the developer package on the STM32MP157D-EV1 board using "Windows os" STM32Cubeprogrammer program?
I even installed the starter package in EMMC boot mode.
And I want to install a developer package.
I want to install SDK, can I use STM32MP157D-EV1 board using STM32Cube Programmer in Windows OS?
Ubuntu 18.04 was installed in virtualbox and STM32Cubeprogrammer was installed. However, the program cannot read the STM32 board on the USB port.
I want to install Ubuntu 18.04 on the STM32MP157D-EV1 board. Is there any way?