Skip to main content
Graduate II
April 18, 2024
Solved

Can STM32MP151 transfer sound via HDMI connector?

  • April 18, 2024
  • 4 replies
  • 3119 views

I'm buildning my own computer by using STM32MP151AAC3.

I'm going to draw lines for the HDMI connector. I have one question: Can I transfer sound via the HDMI cable? For example if I run OpenSTLinux onto the STM32MP151AAC3 processor, and then I connect the HDMI cable and I can see the screen. Will I be able to hear sound too if I surf into Youtube?

    This topic has been closed for replies.
    Best answer by DMårt

    @PatrickF 

    Hi!

    I solved the problem. Now I can hear sound from my SII9022A PHY.

    I did not use ASoC Graph Card, instead I used Simple Card inside Linux kernel.

    I post the Linux Device Tree in case if some one in the future want to play some music through the SII9022A.

     

    // SPDX-License-Identifier: (GPL-2.0-or-later OR BSD-3-Clause)
    /*
     * Copyright (C) 2024, STMicroelectronics - All Rights Reserved
     * Author: STM32CubeMX code generation for STMicroelectronics.
     */
    
    /* For more information on Device Tree configuration, please refer to
     * https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
     */
    
    /dts-v1/;
    
    #include <dt-bindings/pinctrl/stm32-pinfunc.h>
    #include "stm32mp151.dtsi"
    #include "stm32mp15xa.dtsi"
    #include "stm32mp15xxac-pinctrl.dtsi"
    #include "stm32mp15-m4-srm.dtsi"
    
    /* USER CODE BEGIN includes */
    #include "stm32mp15-scmi.dtsi"
    #include <dt-bindings/gpio/gpio.h>
    #include <dt-bindings/mfd/st,stpmic1.h>
    /* USER CODE END includes */
    
    / {
    	model = "STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mpu-v24.06.26";
    	compatible = "st,stm32mp151a-stm32-computer-firmware-mx", "st,stm32mp151";
    
    	memory@c0000000 {
    		device_type = "memory";
    		reg = <0xc0000000 0x20000000>;
    
    		/* USER CODE BEGIN memory */
    		/* USER CODE END memory */
    	};
    
    	reserved-memory {
    		#address-cells = <1>;
    		#size-cells = <1>;
    		ranges;
    
    		/* USER CODE BEGIN reserved-memory */
    		optee@de000000 {
    			reg = <0xde000000 0x2000000>;
    			no-map;
    		};
    		
    		mcuram2:mcuram2@10000000{
    			compatible = "shared-dma-pool";
    			reg = <0x10000000 0x40000>;
    			no-map;
    		};
    
    		vdev0vring0:vdev0vring0@10040000{
    			compatible = "shared-dma-pool";
    			reg = <0x10040000 0x1000>;
    			no-map;
    		};
    
    		vdev0vring1:vdev0vring1@10041000{
    			compatible = "shared-dma-pool";
    			reg = <0x10041000 0x1000>;
    			no-map;
    		};
    
    		vdev0buffer:vdev0buffer@10042000{
    			compatible = "shared-dma-pool";
    			reg = <0x10042000 0x4000>;
    			no-map;
    		};
    
    		mcu_rsc_table:mcu-rsc-table@10048000{
    			compatible = "shared-dma-pool";
    			reg = <0x10048000 0x8000>;
    			no-map;
    		};
    
    		mcuram:mcuram@30000000{
    			compatible = "shared-dma-pool";
    			reg = <0x30000000 0x40000>;
    			no-map;
    		};
    
    		retram:retram@38000000{
    			compatible = "shared-dma-pool";
    			reg = <0x38000000 0x10000>;
    			no-map;
    		};
    		/* USER CODE END reserved-memory */
    	};
    
    	/* USER CODE BEGIN root */
    	aliases{
    		ethernet0 = &ethernet0;
    		serial0 = &uart4;
    	};
    
    	hdmi:connector{
    		compatible = "hdmi-connector";
    		#sound-dai-cells = <0>;
    		label = "hdmi";
    		type = "a";
    
    		port{
    			hdmi_connector_in:endpoint{
    				remote-endpoint = <&sii9022_out>;
    			};
    			hdmi_audio_out:endpoit{
    				remote-endpoint= <&sii9022_tx_endpoint>;
    			};
    		};
    	};
    	
    	sound {
    		compatible = "simple-audio-card";
    		simple-audio-card,name = "SII9022A HDMI";
    		simple-audio-card,format = "i2s";
    		/*simple-audio-card,widgets = "Speaker", "External Speaker";
    		simple-audio-card,routing = "External Speaker", "LINE_OUT";*/
    		simple-audio-card,bitclock-master = <&dailink0_master>;
    		simple-audio-card,frame-master = <&dailink0_master>;
    		simple-audio-card,mclk-fs = <256>;
    		
    		dailink0_master: simple-audio-card,cpu {
    			sound-dai = <&i2s2>;
    		};
    		
    		simple-audio-card,codec {
    			sound-dai = <&sii9022A>;
    		};
    	};
    	
    	config {
    		u-boot,boot-led = "heartbeat";
    		u-boot,error-led = "error";
    		u-boot,mmc-env-partition = "u-boot-env";
    		st,fastboot-gpios = <&gpioa 13 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
    		st,stm32prog-gpios = <&gpioa 14 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
    	};
    
    	led{
    		compatible = "gpio-leds";
    
    		led-blue{
    			label = "heartbeat";
    			gpios = <&gpioa 14 GPIO_ACTIVE_LOW>;
    			linux,default-trigger = "timer"; /* Change from heartbeat -> timer */
    			default-state = "off";
    		};
    		
    		led-red {
    			label = "error";
    			gpios = <&gpioa 13 GPIO_ACTIVE_LOW>;
    			default-state = "off";
    		};
    	};
    	
    	vin:vin{
    		compatible = "regulator-fixed";
    		regulator-name = "vin";
    		regulator-min-microvolt = <5000000>;
    		regulator-max-microvolt = <5000000>;
    		regulator-always-on;
    	};
    
    	chosen{
    		stdout-path = "serial0:115200n8";
    	};
    	/* USER CODE END root */
    
    	clocks{
    
    		/* USER CODE BEGIN clocks */
    		clk_csi: clk-csi {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <4000000>;
    		};
    
    		clk_hse: clk-hse {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <24000000>;
    		};
    
    		clk_hsi: clk-hsi {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <64000000>;
    		};
    
    		clk_lse: clk-lse {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <32768>;
    		};
    
    		clk_lsi: clk-lsi {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <32000>;
    		};
    		/* USER CODE END clocks */
    	};
    
    }; /*root*/
    
    &pinctrl {
    
    	eth1_pins_mx: eth1_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_RX_CLK */
    					 <STM32_PINMUX('A', 7, AF11)>, /* ETH1_RX_CTL */
    					 <STM32_PINMUX('B', 0, AF11)>, /* ETH1_RXD2 */
    					 <STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
    					 <STM32_PINMUX('C', 5, AF11)>, /* ETH1_RXD1 */
    					 <STM32_PINMUX('H', 7, AF11)>; /* ETH1_RXD3 */
    			bias-disable;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <0>;
    		};
    		pins3 {
    			pinmux = <STM32_PINMUX('B', 11, AF11)>, /* ETH1_TX_CTL */
    					 <STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
    					 <STM32_PINMUX('C', 2, AF11)>, /* ETH1_TXD2 */
    					 <STM32_PINMUX('E', 2, AF11)>, /* ETH1_TXD3 */
    					 <STM32_PINMUX('G', 4, AF11)>, /* ETH1_GTX_CLK */
    					 <STM32_PINMUX('G', 5, AF11)>, /* ETH1_CLK125 */
    					 <STM32_PINMUX('G', 13, AF11)>, /* ETH1_TXD0 */
    					 <STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <2>;
    		};
    		pins4 {
    			pinmux = <STM32_PINMUX('B', 5, AF0)>; /* ETH1_CLK */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    	};
    
    	eth1_sleep_pins_mx: eth1_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 1, ANALOG)>, /* ETH1_RX_CLK */
    					 <STM32_PINMUX('A', 2, ANALOG)>, /* ETH1_MDIO */
    					 <STM32_PINMUX('A', 7, ANALOG)>, /* ETH1_RX_CTL */
    					 <STM32_PINMUX('B', 0, ANALOG)>, /* ETH1_RXD2 */
    					 <STM32_PINMUX('B', 5, ANALOG)>, /* ETH1_CLK */
    					 <STM32_PINMUX('B', 11, ANALOG)>, /* ETH1_TX_CTL */
    					 <STM32_PINMUX('C', 1, ANALOG)>, /* ETH1_MDC */
    					 <STM32_PINMUX('C', 2, ANALOG)>, /* ETH1_TXD2 */
    					 <STM32_PINMUX('C', 4, ANALOG)>, /* ETH1_RXD0 */
    					 <STM32_PINMUX('C', 5, ANALOG)>, /* ETH1_RXD1 */
    					 <STM32_PINMUX('E', 2, ANALOG)>, /* ETH1_TXD3 */
    					 <STM32_PINMUX('G', 4, ANALOG)>, /* ETH1_GTX_CLK */
    					 <STM32_PINMUX('G', 5, ANALOG)>, /* ETH1_CLK125 */
    					 <STM32_PINMUX('G', 13, ANALOG)>, /* ETH1_TXD0 */
    					 <STM32_PINMUX('G', 14, ANALOG)>, /* ETH1_TXD1 */
    					 <STM32_PINMUX('H', 7, ANALOG)>; /* ETH1_RXD3 */
    		};
    	};
    
    	hdmi_cec_pins_mx: hdmi_cec_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('B', 6, AF5)>; /* CEC */
    			bias-disable;
    			drive-open-drain;
    			slew-rate = <0>;
    		};
    	};
    
    	hdmi_cec_sleep_pins_mx: hdmi_cec_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('B', 6, ANALOG)>; /* CEC */
    		};
    	};
    
    	i2c1_pins_mx: i2c1_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('D', 12, AF5)>, /* I2C1_SCL */
    					 <STM32_PINMUX('D', 13, AF5)>; /* I2C1_SDA */
    			bias-disable;
    			drive-open-drain;
    			slew-rate = <0>;
    		};
    	};
    
    	i2c1_sleep_pins_mx: i2c1_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('D', 12, ANALOG)>, /* I2C1_SCL */
    					 <STM32_PINMUX('D', 13, ANALOG)>; /* I2C1_SDA */
    		};
    	};
    
    	i2c4_pins_mx: i2c4_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('F', 14, AF4)>, /* I2C4_SCL */
    					 <STM32_PINMUX('F', 15, AF4)>; /* I2C4_SDA */
    			bias-disable;
    			drive-open-drain;
    			slew-rate = <0>;
    		};
    	};
    
    	i2c4_sleep_pins_mx: i2c4_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('F', 14, ANALOG)>, /* I2C4_SCL */
    					 <STM32_PINMUX('F', 15, ANALOG)>; /* I2C4_SDA */
    		};
    	};
    
    	i2s2_pins_mx: i2s2_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 9, AF5)>, /* I2S2_CK */
    					 <STM32_PINMUX('B', 12, AF5)>, /* I2S2_WS */
    					 <STM32_PINMUX('I', 3, AF5)>; /* I2S2_SDO */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    	};
    
    	i2s2_sleep_pins_mx: i2s2_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 9, ANALOG)>, /* I2S2_CK */
    					 <STM32_PINMUX('B', 12, ANALOG)>, /* I2S2_WS */
    					 <STM32_PINMUX('I', 3, ANALOG)>; /* I2S2_SDO */
    		};
    	};
    
    	ltdc_pins_mx: ltdc_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('A', 3, AF14)>, /* LTDC_B5 */
    					 <STM32_PINMUX('B', 1, AF14)>, /* LTDC_G0 */
    					 <STM32_PINMUX('B', 8, AF14)>, /* LTDC_B6 */
    					 <STM32_PINMUX('C', 0, AF14)>, /* LTDC_R5 */
    					 <STM32_PINMUX('D', 8, AF14)>, /* LTDC_B7 */
    					 <STM32_PINMUX('D', 9, AF14)>, /* LTDC_B0 */
    					 <STM32_PINMUX('D', 10, AF14)>, /* LTDC_B3 */
    					 <STM32_PINMUX('E', 6, AF14)>, /* LTDC_G1 */
    					 <STM32_PINMUX('E', 15, AF14)>, /* LTDC_R7 */
    					 <STM32_PINMUX('F', 10, AF14)>, /* LTDC_DE */
    					 <STM32_PINMUX('G', 10, AF14)>, /* LTDC_B2 */
    					 <STM32_PINMUX('G', 12, AF14)>, /* LTDC_B1 */
    					 <STM32_PINMUX('H', 2, AF14)>, /* LTDC_R0 */
    					 <STM32_PINMUX('H', 3, AF14)>, /* LTDC_R1 */
    					 <STM32_PINMUX('H', 8, AF14)>, /* LTDC_R2 */
    					 <STM32_PINMUX('H', 9, AF14)>, /* LTDC_R3 */
    					 <STM32_PINMUX('H', 10, AF14)>, /* LTDC_R4 */
    					 <STM32_PINMUX('H', 12, AF14)>, /* LTDC_R6 */
    					 <STM32_PINMUX('H', 13, AF14)>, /* LTDC_G2 */
    					 <STM32_PINMUX('H', 14, AF14)>, /* LTDC_G3 */
    					 <STM32_PINMUX('H', 15, AF14)>, /* LTDC_G4 */
    					 <STM32_PINMUX('I', 0, AF14)>, /* LTDC_G5 */
    					 <STM32_PINMUX('I', 1, AF14)>, /* LTDC_G6 */
    					 <STM32_PINMUX('I', 2, AF14)>, /* LTDC_G7 */
    					 <STM32_PINMUX('I', 4, AF14)>, /* LTDC_B4 */
    					 <STM32_PINMUX('I', 9, AF14)>, /* LTDC_VSYNC */
    					 <STM32_PINMUX('I', 10, AF14)>; /* LTDC_HSYNC */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <0>;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('G', 7, AF14)>; /* LTDC_CLK */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    	};
    
    	ltdc_sleep_pins_mx: ltdc_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 3, ANALOG)>, /* LTDC_B5 */
    					 <STM32_PINMUX('B', 1, ANALOG)>, /* LTDC_G0 */
    					 <STM32_PINMUX('B', 8, ANALOG)>, /* LTDC_B6 */
    					 <STM32_PINMUX('C', 0, ANALOG)>, /* LTDC_R5 */
    					 <STM32_PINMUX('D', 8, ANALOG)>, /* LTDC_B7 */
    					 <STM32_PINMUX('D', 9, ANALOG)>, /* LTDC_B0 */
    					 <STM32_PINMUX('D', 10, ANALOG)>, /* LTDC_B3 */
    					 <STM32_PINMUX('E', 6, ANALOG)>, /* LTDC_G1 */
    					 <STM32_PINMUX('E', 15, ANALOG)>, /* LTDC_R7 */
    					 <STM32_PINMUX('F', 10, ANALOG)>, /* LTDC_DE */
    					 <STM32_PINMUX('G', 7, ANALOG)>, /* LTDC_CLK */
    					 <STM32_PINMUX('G', 10, ANALOG)>, /* LTDC_B2 */
    					 <STM32_PINMUX('G', 12, ANALOG)>, /* LTDC_B1 */
    					 <STM32_PINMUX('H', 2, ANALOG)>, /* LTDC_R0 */
    					 <STM32_PINMUX('H', 3, ANALOG)>, /* LTDC_R1 */
    					 <STM32_PINMUX('H', 8, ANALOG)>, /* LTDC_R2 */
    					 <STM32_PINMUX('H', 9, ANALOG)>, /* LTDC_R3 */
    					 <STM32_PINMUX('H', 10, ANALOG)>, /* LTDC_R4 */
    					 <STM32_PINMUX('H', 12, ANALOG)>, /* LTDC_R6 */
    					 <STM32_PINMUX('H', 13, ANALOG)>, /* LTDC_G2 */
    					 <STM32_PINMUX('H', 14, ANALOG)>, /* LTDC_G3 */
    					 <STM32_PINMUX('H', 15, ANALOG)>, /* LTDC_G4 */
    					 <STM32_PINMUX('I', 0, ANALOG)>, /* LTDC_G5 */
    					 <STM32_PINMUX('I', 1, ANALOG)>, /* LTDC_G6 */
    					 <STM32_PINMUX('I', 2, ANALOG)>, /* LTDC_G7 */
    					 <STM32_PINMUX('I', 4, ANALOG)>, /* LTDC_B4 */
    					 <STM32_PINMUX('I', 9, ANALOG)>, /* LTDC_VSYNC */
    					 <STM32_PINMUX('I', 10, ANALOG)>; /* LTDC_HSYNC */
    		};
    	};
    
    	sdmmc2_pins_mx: sdmmc2_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
    					 <STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
    					 <STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
    					 <STM32_PINMUX('B', 9, AF10)>, /* SDMMC2_D5 */
    					 <STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
    					 <STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
    					 <STM32_PINMUX('E', 5, AF9)>; /* SDMMC2_D6 */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
    					 <STM32_PINMUX('E', 3, AF9)>, /* SDMMC2_CK */
    					 <STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
    			bias-pull-up;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    	};
    
    	sdmmc2_opendrain_pins_mx: sdmmc2_opendrain_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
    					 <STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
    					 <STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
    					 <STM32_PINMUX('B', 9, AF10)>, /* SDMMC2_D5 */
    					 <STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
    					 <STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
    					 <STM32_PINMUX('E', 5, AF9)>; /* SDMMC2_D6 */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
    					 <STM32_PINMUX('E', 3, AF9)>; /* SDMMC2_CK */
    			bias-pull-up;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    		pins3 {
    			pinmux = <STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
    			bias-pull-up;
    			drive-open-drain;
    			slew-rate = <1>;
    		};
    	};
    
    	sdmmc2_sleep_pins_mx: sdmmc2_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 8, ANALOG)>, /* SDMMC2_D4 */
    					 <STM32_PINMUX('B', 3, ANALOG)>, /* SDMMC2_D2 */
    					 <STM32_PINMUX('B', 4, ANALOG)>, /* SDMMC2_D3 */
    					 <STM32_PINMUX('B', 9, ANALOG)>, /* SDMMC2_D5 */
    					 <STM32_PINMUX('B', 14, ANALOG)>, /* SDMMC2_D0 */
    					 <STM32_PINMUX('B', 15, ANALOG)>, /* SDMMC2_D1 */
    					 <STM32_PINMUX('C', 7, ANALOG)>, /* SDMMC2_D7 */
    					 <STM32_PINMUX('E', 3, ANALOG)>, /* SDMMC2_CK */
    					 <STM32_PINMUX('E', 5, ANALOG)>, /* SDMMC2_D6 */
    					 <STM32_PINMUX('G', 6, ANALOG)>; /* SDMMC2_CMD */
    		};
    	};
    
    	uart4_pins_mx: uart4_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */
    			bias-pull-up;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('G', 11, AF6)>; /* UART4_TX */
    			bias-pull-up;
    			drive-push-pull;
    			slew-rate = <0>;
    		};
    	};
    
    	uart4_idle_pins_mx: uart4_idle_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */
    			bias-pull-up;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('G', 11, ANALOG)>; /* UART4_TX */
    			bias-pull-up;
    		};
    	};
    
    	uart4_sleep_pins_mx: uart4_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('B', 2, ANALOG)>, /* UART4_RX */
    					 <STM32_PINMUX('G', 11, ANALOG)>; /* UART4_TX */
    			bias-pull-up;
    		};
    	};
    
    	usb_otg_hs_pins_mx: usb_otg_hs_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 10, ANALOG)>; /* USB_OTG_HS_ID */
    		};
    	};
    
    	usb_otg_hs_sleep_pins_mx: usb_otg_hs_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 10, ANALOG)>; /* USB_OTG_HS_ID */
    		};
    	};
    
    	/* USER CODE BEGIN pinctrl */
    	/* USER CODE END pinctrl */
    };
    
    &pinctrl_z {
    
    	/* USER CODE BEGIN pinctrl_z */
    	/* USER CODE END pinctrl_z */
    };
    
    &m4_rproc{
    	status = "disabled";
    
    	/* USER CODE BEGIN m4_rproc */
    	resets = <&scmi_reset RST_SCMI_MCU>, <&scmi_reset RST_SCMI_MCU_HOLD_BOOT>;
    	reset-names = "mcu_rst", "hold_boot";
    	/*/delete-property/ st,syscfg-holdboot;*/
    	mboxes = <&ipcc 0>, <&ipcc 1>, <&ipcc 2>, <&ipcc 3>;
    	mbox-names = "vq0", "vq1", "shutdown", "detach";
    	memory-region = <&retram>, <&mcuram>, <&mcuram2>, <&vdev0vring0>, <&vdev0vring1>, <&vdev0buffer>, <&mcu_rsc_table>;
    	interrupt-parent = <&exti>;
    	interrupts = <68 1>;
    	wakeup-source;
    	/* USER CODE END m4_rproc */
    
    	m4_system_resources{
    		status = "disabled";
    
    		/* USER CODE BEGIN m4_system_resources */
    		/* USER CODE END m4_system_resources */
    	};
    };
    
    &bsec{
    	status = "okay";
    
    	/* USER CODE BEGIN bsec */
    	/* USER CODE END bsec */
    };
    
    &cec{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&hdmi_cec_pins_mx>;
    	pinctrl-1 = <&hdmi_cec_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN cec */
    	/* USER CODE END cec */
    };
    
    &dma1{
    	status = "okay";
    
    	/* USER CODE BEGIN dma1 */
    	resets = <&scmi_reset RST_SCMI_MDMA>;
    	/* USER CODE END dma1 */
    };
    
    &dma2{
    	status = "disabled";
    
    	/* USER CODE BEGIN dma2 */
    	/* USER CODE END dma2 */
    };
    
    &dmamux1{
    	status = "okay";
    
    	dma-masters = <&dma1>;
    	dma-channels = <8>;
    
    	/* USER CODE BEGIN dmamux1 */
    	/* USER CODE END dmamux1 */
    };
    
    &ethernet0{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&eth1_pins_mx>;
    	pinctrl-1 = <&eth1_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN ethernet0 */
    	phy-mode = "rgmii-id";
    	max-speed = <1000>;
    	phy-handle = <&phy0>;
    	nvmem-cells = <&ethernet_mac_address>;
    	nvmem-cell-names = "mac-address";
    
    	mdio{
    		#address-cells = <1>;
    		#size-cells = <0>;
    		compatible = "snps,dwmac-mdio";
    
    		phy0:ethernet-phy@0{
    			reg = <0>;
    		};
    	};
    	/* USER CODE END ethernet0 */
    };
    
    &hsem{
    	status = "okay";
    
    	/* USER CODE BEGIN hsem */
    	/* USER CODE END hsem */
    };
    
    &i2c1{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&i2c1_pins_mx>;
    	pinctrl-1 = <&i2c1_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN i2c1 */
    	/* USER CODE END i2c1 */
    };
    
    &i2c4{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&i2c4_pins_mx>;
    	pinctrl-1 = <&i2c4_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN i2c4 */
    	clocks = <&scmi_clk CK_SCMI_I2C4>;
    	resets = <&scmi_reset RST_SCMI_I2C4>;
    	i2c-scl-rising-time-ns = <185>;
    	i2c-scl-falling-time-ns = <20>;
    	clock-frequency = <400000>;
    	/delete-property/ dmas;
    	/delete-property/ dma-names;
    
    	sii9022A: hdmi-transmitter@39{
    		compatible = "sil,sii9022";
    		reg = <0x39>;
    		iovcc-supply = <&v3v3_hdmi>;
    		cvcc12-supply = <&v1v2_hdmi>;
    		reset-gpios = <&gpioe 8 GPIO_ACTIVE_LOW>;
    		interrupts = <1 IRQ_TYPE_EDGE_FALLING>;
    		interrupt-parent = <&gpiog>;
    		#sound-dai-cells = <0>;
    		sil,i2s-data-lanes = <0>;
    		/*clocks = <&mclk>;
    		clock-names = "mclk";*/
    		status = "okay";
    
    		ports{
    			#address-cells = <1>;
    			#size-cells = <0>;
    
    			port@0{
    				reg = <0>;
    
    				sii9022_in:endpoint{
    					remote-endpoint = <&ltdc_ep0_out>;
    				};
    			};
    
    			port@1{
    				reg = <1>;
    
    				sii9022_out:endpoint{
    					remote-endpoint = <&hdmi_connector_in>;
    				};
    			};
    
    			port@3{
    				reg = <3>;
    
    				sii9022_tx_endpoint:endpoint{
    					remote-endpoint = <&i2s2_endpoint>;
    				};
    			};
    		};
    	};
    	
    	pmic:stpmic@33{
    		compatible = "st,stpmic1";
    		reg = <0x33>;
    		/*interrupts-extended = <&gpioa 0 IRQ_TYPE_EDGE_FALLING>;*/
    		interrupts-extended = <&exti 55 IRQ_TYPE_EDGE_FALLING>;
    		interrupt-controller;
    		#interrupt-cells = <2>;
    		status = "okay";
    
    		regulators{
    			compatible = "st,stpmic1-regulators";
    			buck1-supply = <&vin>;
    			buck2-supply = <&vin>;
    			buck3-supply = <&vin>;
    			buck4-supply = <&vin>;
    			/*ldo1-supply = <&v3v3>;*/
    			ldo2-supply = <&vin>;
    			ldo3-supply = <&vdd_ddr>;
    			ldo4-supply = <&vin>;
    			ldo5-supply = <&vin>;
    			ldo6-supply = <&v3v3>;
    			vref_ddr-supply = <&vin>;
    			/*boost-supply = <&vin>;
    			pwr_sw1-supply = <&bst_out>;
    			pwr_sw2-supply = <&bst_out>;*/
    
    			vddcore:buck1{
    				regulator-name = "vddcore";
    				regulator-min-microvolt = <1200000>;
    				regulator-max-microvolt = <1350000>;
    				regulator-always-on;
    				regulator-initial-mode = <0>;
    				regulator-over-current-protection;
    			};
    
    			vdd_ddr:buck2{
    				regulator-name = "vdd_ddr";
    				regulator-min-microvolt = <1350000>;
    				regulator-max-microvolt = <1350000>;
    				regulator-always-on;
    				regulator-initial-mode = <0>;
    				regulator-over-current-protection;
    			};
    
    			vdd:buck3{
    				regulator-name = "vdd";
    				regulator-min-microvolt = <3300000>;
    				regulator-max-microvolt = <3300000>;
    				regulator-always-on;
    				st,mask-reset;
    				regulator-initial-mode = <0>;
    				regulator-over-current-protection;
    			};
    
    			v3v3:buck4{
    				regulator-name = "v3v3";
    				regulator-min-microvolt = <3300000>;
    				regulator-max-microvolt = <3300000>;
    				regulator-always-on;
    				regulator-over-current-protection;
    				regulator-initial-mode = <0>;
    			};
    			
    			/*
    			v1v8_audio:ldo1{
    				regulator-name = "v1v8_audio";
    				regulator-min-microvolt = <1800000>;
    				regulator-max-microvolt = <1800000>;
    				regulator-always-on;
    				interrupts = <IT_CURLIM_LDO1 0>;
    			};*/
    
    			v3v3_hdmi:ldo2{
    				regulator-name = "v3v3_hdmi";
    				regulator-min-microvolt = <3300000>;
    				regulator-max-microvolt = <3300000>;
    				regulator-always-on;
    				interrupts = <IT_CURLIM_LDO2 0>;
    			};
    
    			vtt_ddr:ldo3{
    				regulator-name = "vtt_ddr";
    				regulator-min-microvolt = <500000>;
    				regulator-max-microvolt = <750000>;
    				regulator-always-on;
    				regulator-over-current-protection;
    			};
    
    			vdd_usb:ldo4{
    				regulator-name = "vdd_usb";
    				interrupts = <IT_CURLIM_LDO4 0>;
    			};
    
    			vdda:ldo5{
    				regulator-name = "vdda";
    				regulator-min-microvolt = <2900000>;
    				regulator-max-microvolt = <2900000>;
    				interrupts = <IT_CURLIM_LDO5 0>;
    				regulator-boot-on;
    			};
    
    			v1v2_hdmi:ldo6{
    				regulator-name = "v1v2_hdmi";
    				regulator-min-microvolt = <1200000>;
    				regulator-max-microvolt = <1200000>;
    				regulator-always-on;
    				interrupts = <IT_CURLIM_LDO6 0>;
    			};
    
    			vref_ddr:vref-ddr{
    				regulator-name = "vref_ddr";
    				regulator-always-on;
    			};
    
    			/*
    			bst_out:boost{
    				regulator-name = "bst_out";
    				interrupts = <IT_OCP_BOOST 0>;
    			};
    
    			vbus_otg:pwr-sw1{
    				regulator-name = "vbus_otg";
    				interrupts = <IT_OCP_OTG 0>;
    			};
    
    			vbus_sw:pwr-sw2{
    				regulator-name = "vbus_sw";
    				interrupts = <IT_OCP_SWOUT 0>;
    				regulator-active-discharge = <1>;
    			};
    			*/
    		};
    
    		onkey{
    			compatible = "st,stpmic1-onkey";
    			interrupts = <IT_PONKEY_F 0>, <IT_PONKEY_R 0>;
    			interrupt-names = "onkey-falling", "onkey-rising";
    			power-off-time-sec = <10>;
    			status = "okay";
    		};
    	};
    	/* USER CODE END i2c4 */
    };
    
    &i2s2{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&i2s2_pins_mx>;
    	pinctrl-1 = <&i2s2_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN i2s2 */
    	clocks = <&rcc SPI2>, <&rcc SPI2_K>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
    	clock-names = "pclk", "i2sclk", "x8k", "x11k";
    
    	i2s2_port:port{
    		i2s2_endpoint:endpoint{
    			remote-endpoint = <&sii9022_tx_endpoint>;
    			dai-format = "i2s";
    			mclk-fs = <256>;
    		};
    	};
    	/* USER CODE END i2s2 */
    };
    
    &ltdc{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&ltdc_pins_mx>;
    	pinctrl-1 = <&ltdc_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN ltdc */
    	port{
    
    		ltdc_ep0_out:endpoint{
    			remote-endpoint = <&sii9022_in>;
    		};
    	};
    	/* USER CODE END ltdc */
    };
    
    &m4_dma2{
    	status = "okay";
    
    	/* USER CODE BEGIN m4_dma2 */
    	/* USER CODE END m4_dma2 */
    };
    
    &mdma1{
    	status = "okay";
    
    	/* USER CODE BEGIN mdma1 */
    	/* USER CODE END mdma1 */
    };
    
    &pwr_regulators{
    	status = "okay";
    
    	/* USER CODE BEGIN pwr_regulators */
    	vdd-supply = <&vdd>;
    	vdd_3v3_usbfs-supply = <&vdd_usb>;
    	/* USER CODE END pwr_regulators */
    };
    
    &rcc{
    	status = "okay";
    
    	/* USER CODE BEGIN rcc */
    	compatible = "st,stm32mp1-rcc-secure", "syscon";
    	clock-names = "hse", "hsi", "csi", "lse", "lsi";
    	clocks = <&scmi_clk CK_SCMI_HSE>,
    		 <&scmi_clk CK_SCMI_HSI>,
    		 <&scmi_clk CK_SCMI_CSI>,
    		 <&scmi_clk CK_SCMI_LSE>,
    		 <&scmi_clk CK_SCMI_LSI>;
    	/* USER CODE END rcc */
    };
    
    &rng1{
    	status = "okay";
    
    	/* USER CODE BEGIN rng1 */
    	clocks = <&scmi_clk CK_SCMI_RNG1>;
    	resets = <&scmi_reset RST_SCMI_RNG1>;
    	/* USER CODE END rng1 */
    };
    
    &rtc{
    	status = "okay";
    
    	/* USER CODE BEGIN rtc */
    	clocks = <&scmi_clk CK_SCMI_RTCAPB>, <&scmi_clk CK_SCMI_RTC>;
    	/* USER CODE END rtc */
    };
    
    &sdmmc2{
    	pinctrl-names = "default", "opendrain", "sleep";
    	pinctrl-0 = <&sdmmc2_pins_mx>;
    	pinctrl-1 = <&sdmmc2_opendrain_pins_mx>;
    	pinctrl-2 = <&sdmmc2_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN sdmmc2 */
    	non-removable;
    	no-sd;
    	no-sdio;
    	st,neg-edge;
    	bus-width = <8>;
    	vmmc-supply = <&v3v3>;
    	vqmmc-supply = <&vdd>;
    	mmc-ddr-3_3v;
    	/* USER CODE END sdmmc2 */
    };
    
    &tamp{
    	status = "okay";
    
    	/* USER CODE BEGIN tamp */
    	/* USER CODE END tamp */
    };
    
    &uart4{
    	pinctrl-names = "default", "idle", "sleep";
    	pinctrl-0 = <&uart4_pins_mx>;
    	pinctrl-1 = <&uart4_idle_pins_mx>;
    	pinctrl-2 = <&uart4_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN uart4 */
    	/delete-property/ dmas;
    	/delete-property/ dma-names;
    	u-boot,dm-pre-reloc;
    	/* USER CODE END uart4 */
    };
    
    &usbh_ehci{
    	status = "okay";
    
    	/* USER CODE BEGIN usbh_ehci */
    	phys = <&usbphyc_port0>;
    	#address-cells = <1>;
    	#size-cells = <0>;
    	/* onboard HUB */
    	hub@1 {
    		compatible = "usb424,2514";
    		reg = <1>;
    		vdd-supply = <&v3v3>;
    	};
    	/* USER CODE END usbh_ehci */
    };
    
    &usbh_ohci{
    	status = "okay";
    
    	/* USER CODE BEGIN usbh_ohci */
    	/* USER CODE END usbh_ohci */
    };
    
    &usbotg_hs{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&usb_otg_hs_pins_mx>;
    	pinctrl-1 = <&usb_otg_hs_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN usbotg_hs */
    	phys = <&usbphyc_port1 0>;
    	phy-names = "usb2-phy";
    	usb-role-switch;
     u-boot,dm-pre-reloc; 
     u-boot,force-b-session-valid;
     hnp-srp-disable;
     dr_mode = "peripheral"; 
    	/* USER CODE END usbotg_hs */
    };
    
    &usbphyc{
    	status = "okay";
    
    	/* USER CODE BEGIN usbphyc */
    	phy-supply = <&vdd_usb>;
    	/* USER CODE END usbphyc */
    };
    
    &usbphyc_port0{
    	status = "okay";
    
    	/* USER CODE BEGIN usbphyc_port0 */
    	phy-supply = <&vdd_usb>;
    	st,tune-hs-dc-level = <2>;
    	st,enable-fs-rftime-tuning;
    	st,enable-hs-rftime-reduction;
    	st,trim-hs-current = <15>;
    	st,trim-hs-impedance = <1>;
    	st,tune-squelch-level = <3>;
    	st,tune-hs-rx-offset = <2>;
    	st,no-lsfs-sc;
    	/* USER CODE END usbphyc_port0 */
    };
    
    &usbphyc_port1{
    	status = "okay";
    
    	/* USER CODE BEGIN usbphyc_port1 */
    	phy-supply = <&vdd_usb>;
    	st,tune-hs-dc-level = <2>;
    	st,enable-fs-rftime-tuning;
    	st,enable-hs-rftime-reduction;
    	st,trim-hs-current = <15>;
    	st,trim-hs-impedance = <1>;
    	st,tune-squelch-level = <3>;
    	st,tune-hs-rx-offset = <2>;
    	st,no-lsfs-sc;
    	/* USER CODE END usbphyc_port1 */
    };
    
    /* USER CODE BEGIN addons */
    /*
    &arm_wdt{
    	timeout-sec = <32>;
    	status = "okay";
    };
    */
    &cpu0 {
    	cpu-supply = <&vddcore>;
    	clocks = <&scmi_clk CK_SCMI_MPU>;
    };
    
    &uart4_pins_mx {
    	u-boot,dm-pre-reloc;
    	pins1 {
    		u-boot,dm-pre-reloc;
    	};
    	pins2 {
    		u-boot,dm-pre-reloc;
    	};
    };
    &gpioz {
    	clocks = <&scmi_clk CK_SCMI_GPIOZ>;
    };
    /* USER CODE END addons */

    4 replies

    Technical Moderator
    April 19, 2024

    Hi @DMårt 

    note that performance of STM32MP151A as general purpose 'computer' might be deceptive. I think you could forget Youtube video thru HTML browsing (e.g. no high-resolution capable and only SW video decoder).

    Anyway, no issue to output audio on HDMI, please refer to STM32MP157F-DK2 reference design.

    Regards.

    DMårtAuthor
    Graduate II
    April 20, 2024

    @PatrickF 

    Thank you for your reply.

    I have no plats to have that STM32MP151AAC3 as a general purpose computer. But I have plans to have a GUI application onto it, written in C or C++ or Java.

    Is that possible? 3D or 2D.

    Technical Moderator
    April 22, 2024

    Hi,

    no issue to have nice GUI with STM32MP151.

    3D is possible, but without GPU and with single-core Cortex-A7, might not be best performances.

    Regards.

    DMårtAuthor
    Graduate II
    October 26, 2024

    Hi @PatrickF 

    Note! What you are refering to is not the HDMI PHY.

    You refering to another IC chip.

    The linux kernel does not support sii9022A without MCLK.

    I get these debug messages from sii902x.c https://github.com/torvalds/linux/blob/master/drivers/gpu/drm/bridge/sii902x.c because my device requries MCLK. I have not routed that track from my MCU to the PHY. So sound won't work for the moment until sii902x.c supports PLL as a clock instead of only MCLK.

     

     

     if (daifmt->bit_clk_provider || daifmt->frame_clk_provider) {
     dev_dbg(dev, "%s: I2S clock provider mode not supported\n", __func__); <--------------------------
     return -EINVAL;
     }
    
     switch (daifmt->fmt) {
     case HDMI_I2S:
     i2s_config_reg |= SII902X_TPI_I2S_FIRST_BIT_SHIFT_YES |
     SII902X_TPI_I2S_SD_JUSTIFY_LEFT;
     break;
     case HDMI_RIGHT_J:
     i2s_config_reg |= SII902X_TPI_I2S_SD_JUSTIFY_RIGHT;
     break;
     case HDMI_LEFT_J:
     i2s_config_reg |= SII902X_TPI_I2S_SD_JUSTIFY_LEFT;
     break;
     default:
     dev_dbg(dev, "%s: Unsupported i2s format %u\n", __func__, daifmt->fmt); <--------------------------------
     return -EINVAL;
     }

     

    Skärmbild 2024-10-24 200554.pngSkärmbild 2024-10-24 200702.png

     

    The device tree requries the mclk.

    https://www.kernel.org/doc/Documentation/devicetree/bindings/display/bridge/sil%2Csii9022.yaml

     

    # SPDX-License-Identifier: (GPL-2.0-only OR BSD-2-Clause)
    %YAML 1.2
    ---
    $id: http://devicetree.org/schemas/display/bridge/sil,sii9022.yaml#
    $schema: http://devicetree.org/meta-schemas/core.yaml#
    
    title: Silicon Image sii902x HDMI bridge
    
    maintainers:
     - Boris Brezillon <bbrezillon@kernel.org>
    
    properties:
     compatible:
     oneOf:
     - items:
     - enum:
     - sil,sii9022-cpi # CEC Programming Interface
     - sil,sii9022-tpi # Transmitter Programming Interface
     - const: sil,sii9022
     - const: sil,sii9022
    
     reg:
     maxItems: 1
    
     interrupts:
     maxItems: 1
     description: Interrupt line used to inform the host about hotplug events.
    
     reset-gpios:
     maxItems: 1
    
     iovcc-supply:
     description: I/O Supply Voltage (1.8V or 3.3V)
    
     cvcc12-supply:
     description: Digital Core Supply Voltage (1.2V)
    
     '#sound-dai-cells':
     enum: [ 0, 1 ]
     description: |
     <0> if only I2S or S/PDIF pin is wired,
     <1> if both are wired.
     HDMI audio is configured only if this property is found.
     If HDMI audio is configured, the sii902x device becomes an I2S and/or
     S/PDIF audio codec component (e.g. a digital audio sink), that can be
     used in configuring full audio devices with simple-card or
     audio-graph-card bindings. See their binding documents on how to describe
     the way the
     sii902x device is connected to the rest of the audio system:
     Documentation/devicetree/bindings/sound/simple-card.yaml
     Documentation/devicetree/bindings/sound/audio-graph-card.yaml
     Note: In case of the audio-graph-card binding the used port index should
     be 3.
    
     sil,i2s-data-lanes:
     $ref: /schemas/types.yaml#/definitions/uint32-array
     minItems: 1
     maxItems: 4
     uniqueItems: true
     items:
     enum: [ 0, 1, 2, 3 ]
     description:
     Each integer indicates which I2S pin is connected to which audio FIFO.
     The first integer selects the I2S audio pin for the first audio FIFO#0
     (HDMI channels 1&2), the second for FIFO#1 (HDMI channels 3&4), and so
     on. There are 4 FIFOs and 4 I2S pins (SD0 - SD3). Any I2S pin can be
     connected to any FIFO, but there can be no gaps. E.g. an I2S pin must be
     mapped to FIFO#0 and FIFO#1 before mapping a channel to FIFO#2. The
     default value is <0>, describing SD0 pin being routed to HDMI audio
     FIFO#0.
    
     clocks:
     maxItems: 1
     description: MCLK input. MCLK can be used to produce HDMI audio CTS values.
    
     clock-names:
     const: mclk
    
     ports:
     $ref: /schemas/graph.yaml#/properties/ports
    
     properties:
     port@0:
     $ref: /schemas/graph.yaml#/properties/port
     description: Parallel RGB input port
    
     port@1:
     $ref: /schemas/graph.yaml#/properties/port
     description: HDMI output port
    
     port@3:
     $ref: /schemas/graph.yaml#/properties/port
     description: Sound input port
    
    required:
     - compatible
     - reg
    
    additionalProperties: false
    
    examples:
     - |
     i2c {
     #address-cells = <1>;
     #size-cells = <0>;
    
     hdmi-bridge@39 {
     compatible = "sil,sii9022";
     reg = <0x39>;
     reset-gpios = <&pioA 1 0>;
     iovcc-supply = <&v3v3_hdmi>;
     cvcc12-supply = <&v1v2_hdmi>;
    
     #sound-dai-cells = <0>;
     sil,i2s-data-lanes = < 0 1 2 >;
     clocks = <&mclk>;
     clock-names = "mclk";
    
     ports {
     #address-cells = <1>;
     #size-cells = <0>;
    
     port@0 {
     reg = <0>;
     bridge_in: endpoint {
     remote-endpoint = <&dc_out>;
     };
     };
     };
     };
     };
    DMårtAuthor
    Graduate II
    October 27, 2024

    Hi @PatrickF 

    I have updated my DT.

    Instead of ASoC Audio Graph Card, I'm using Simple Sound Card instead. It seems like I can get a hdmi-audio-codec and ha i2s-hifi...I don't know what they are doing.

    DMrt_0-1730068594656.png

     

    / { 
    	hdmi:connector{
    		compatible = "hdmi-connector";
    		#sound-dai-cells = <0>;
    		label = "hdmi";
    		type = "a";
    
    		port{
    			hdmi_connector_in:endpoint{
    				remote-endpoint = <&sii9022_out>;
    			};
     hdmi_audio_out:endpoit{
    				remote-endpoint= <&sii9022_tx_endpoint>;
    			};
    		};
    	};
    	
    	sound {
    		compatible = "simple-audio-card";
    		simple-audio-card,name = "SII9022A HDMI";
    		simple-audio-card,format = "i2s";
    		simple-audio-card,widgets = "Speaker", "External Speaker";
    		simple-audio-card,routing = "External Speaker", "LINE_OUT";
    		simple-audio-card,bitclock-master = <&dailink0_master>;
    		simple-audio-card,frame-master = <&dailink0_master>;
    		
    		simple-audio-card,cpu {
    			sound-dai = <&i2s2>;
    		};
    		
    		dailink0_master: simple-audio-card,codec {
    			sound-dai = <&hdmi>;
    		};
    	};
    };
    
    &i2c4{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&i2c4_pins_mx>;
    	pinctrl-1 = <&i2c4_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN i2c4 */
    	clocks = <&scmi_clk CK_SCMI_I2C4>;
    	resets = <&scmi_reset RST_SCMI_I2C4>;
    	i2c-scl-rising-time-ns = <185>;
    	i2c-scl-falling-time-ns = <20>;
    	clock-frequency = <400000>;
    	/delete-property/ dmas;
    	/delete-property/ dma-names;
    
     hdmi-transmitter@39{
    		compatible = "sil,sii9022";
    		reg = <0x39>;
    		iovcc-supply = <&v3v3_hdmi>;
    		cvcc12-supply = <&v1v2_hdmi>;
    		reset-gpios = <&gpioe 8 GPIO_ACTIVE_LOW>;
    		interrupts = <1 IRQ_TYPE_EDGE_FALLING>;
    		interrupt-parent = <&gpiog>;
    		#sound-dai-cells = <0>;
    		sil,i2s-data-lanes = <0>;
    		/*clocks = <&mclk>;
    		clock-names = "mclk";*/
    		status = "okay";
    
    		ports{
    			#address-cells = <1>;
    			#size-cells = <0>;
    
    			port@0{
    				reg = <0>;
    
    				sii9022_in:endpoint{
    					remote-endpoint = <&ltdc_ep0_out>;
    				};
    			};
    
    			port@1{
    				reg = <1>;
    
    				sii9022_out:endpoint{
    					remote-endpoint = <&hdmi_connector_in>;
    				};
    			};
    
    			port@3{
    				reg = <3>;
    
    				sii9022_tx_endpoint:endpoint{
    					remote-endpoint = <&i2s2_endpoint>;
    				};
    			};
    		};
    	};
    };
    
    &i2s2{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&i2s2_pins_mx>;
    	pinctrl-1 = <&i2s2_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN i2s2 */
    	clocks = <&rcc SPI2>, <&rcc SPI2_K>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
    	clock-names = "pclk", "i2sclk", "x8k", "x11k";
    
    	i2s2_port:port{
    		i2s2_endpoint:endpoint{
    			remote-endpoint = <&sii9022_tx_endpoint>;
    			dai-format = "i2s";
    			mclk-fs = <256>;
    		};
    	};
    	/* USER CODE END i2s2 */
    };

     

     

    DMårtAuthorAnswer
    Graduate II
    October 29, 2024

    @PatrickF 

    Hi!

    I solved the problem. Now I can hear sound from my SII9022A PHY.

    I did not use ASoC Graph Card, instead I used Simple Card inside Linux kernel.

    I post the Linux Device Tree in case if some one in the future want to play some music through the SII9022A.

     

    // SPDX-License-Identifier: (GPL-2.0-or-later OR BSD-3-Clause)
    /*
     * Copyright (C) 2024, STMicroelectronics - All Rights Reserved
     * Author: STM32CubeMX code generation for STMicroelectronics.
     */
    
    /* For more information on Device Tree configuration, please refer to
     * https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
     */
    
    /dts-v1/;
    
    #include <dt-bindings/pinctrl/stm32-pinfunc.h>
    #include "stm32mp151.dtsi"
    #include "stm32mp15xa.dtsi"
    #include "stm32mp15xxac-pinctrl.dtsi"
    #include "stm32mp15-m4-srm.dtsi"
    
    /* USER CODE BEGIN includes */
    #include "stm32mp15-scmi.dtsi"
    #include <dt-bindings/gpio/gpio.h>
    #include <dt-bindings/mfd/st,stpmic1.h>
    /* USER CODE END includes */
    
    / {
    	model = "STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mpu-v24.06.26";
    	compatible = "st,stm32mp151a-stm32-computer-firmware-mx", "st,stm32mp151";
    
    	memory@c0000000 {
    		device_type = "memory";
    		reg = <0xc0000000 0x20000000>;
    
    		/* USER CODE BEGIN memory */
    		/* USER CODE END memory */
    	};
    
    	reserved-memory {
    		#address-cells = <1>;
    		#size-cells = <1>;
    		ranges;
    
    		/* USER CODE BEGIN reserved-memory */
    		optee@de000000 {
    			reg = <0xde000000 0x2000000>;
    			no-map;
    		};
    		
    		mcuram2:mcuram2@10000000{
    			compatible = "shared-dma-pool";
    			reg = <0x10000000 0x40000>;
    			no-map;
    		};
    
    		vdev0vring0:vdev0vring0@10040000{
    			compatible = "shared-dma-pool";
    			reg = <0x10040000 0x1000>;
    			no-map;
    		};
    
    		vdev0vring1:vdev0vring1@10041000{
    			compatible = "shared-dma-pool";
    			reg = <0x10041000 0x1000>;
    			no-map;
    		};
    
    		vdev0buffer:vdev0buffer@10042000{
    			compatible = "shared-dma-pool";
    			reg = <0x10042000 0x4000>;
    			no-map;
    		};
    
    		mcu_rsc_table:mcu-rsc-table@10048000{
    			compatible = "shared-dma-pool";
    			reg = <0x10048000 0x8000>;
    			no-map;
    		};
    
    		mcuram:mcuram@30000000{
    			compatible = "shared-dma-pool";
    			reg = <0x30000000 0x40000>;
    			no-map;
    		};
    
    		retram:retram@38000000{
    			compatible = "shared-dma-pool";
    			reg = <0x38000000 0x10000>;
    			no-map;
    		};
    		/* USER CODE END reserved-memory */
    	};
    
    	/* USER CODE BEGIN root */
    	aliases{
    		ethernet0 = &ethernet0;
    		serial0 = &uart4;
    	};
    
    	hdmi:connector{
    		compatible = "hdmi-connector";
    		#sound-dai-cells = <0>;
    		label = "hdmi";
    		type = "a";
    
    		port{
    			hdmi_connector_in:endpoint{
    				remote-endpoint = <&sii9022_out>;
    			};
    			hdmi_audio_out:endpoit{
    				remote-endpoint= <&sii9022_tx_endpoint>;
    			};
    		};
    	};
    	
    	sound {
    		compatible = "simple-audio-card";
    		simple-audio-card,name = "SII9022A HDMI";
    		simple-audio-card,format = "i2s";
    		/*simple-audio-card,widgets = "Speaker", "External Speaker";
    		simple-audio-card,routing = "External Speaker", "LINE_OUT";*/
    		simple-audio-card,bitclock-master = <&dailink0_master>;
    		simple-audio-card,frame-master = <&dailink0_master>;
    		simple-audio-card,mclk-fs = <256>;
    		
    		dailink0_master: simple-audio-card,cpu {
    			sound-dai = <&i2s2>;
    		};
    		
    		simple-audio-card,codec {
    			sound-dai = <&sii9022A>;
    		};
    	};
    	
    	config {
    		u-boot,boot-led = "heartbeat";
    		u-boot,error-led = "error";
    		u-boot,mmc-env-partition = "u-boot-env";
    		st,fastboot-gpios = <&gpioa 13 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
    		st,stm32prog-gpios = <&gpioa 14 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
    	};
    
    	led{
    		compatible = "gpio-leds";
    
    		led-blue{
    			label = "heartbeat";
    			gpios = <&gpioa 14 GPIO_ACTIVE_LOW>;
    			linux,default-trigger = "timer"; /* Change from heartbeat -> timer */
    			default-state = "off";
    		};
    		
    		led-red {
    			label = "error";
    			gpios = <&gpioa 13 GPIO_ACTIVE_LOW>;
    			default-state = "off";
    		};
    	};
    	
    	vin:vin{
    		compatible = "regulator-fixed";
    		regulator-name = "vin";
    		regulator-min-microvolt = <5000000>;
    		regulator-max-microvolt = <5000000>;
    		regulator-always-on;
    	};
    
    	chosen{
    		stdout-path = "serial0:115200n8";
    	};
    	/* USER CODE END root */
    
    	clocks{
    
    		/* USER CODE BEGIN clocks */
    		clk_csi: clk-csi {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <4000000>;
    		};
    
    		clk_hse: clk-hse {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <24000000>;
    		};
    
    		clk_hsi: clk-hsi {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <64000000>;
    		};
    
    		clk_lse: clk-lse {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <32768>;
    		};
    
    		clk_lsi: clk-lsi {
    			#clock-cells = <0>;
    			compatible = "fixed-clock";
    			clock-frequency = <32000>;
    		};
    		/* USER CODE END clocks */
    	};
    
    }; /*root*/
    
    &pinctrl {
    
    	eth1_pins_mx: eth1_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_RX_CLK */
    					 <STM32_PINMUX('A', 7, AF11)>, /* ETH1_RX_CTL */
    					 <STM32_PINMUX('B', 0, AF11)>, /* ETH1_RXD2 */
    					 <STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
    					 <STM32_PINMUX('C', 5, AF11)>, /* ETH1_RXD1 */
    					 <STM32_PINMUX('H', 7, AF11)>; /* ETH1_RXD3 */
    			bias-disable;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <0>;
    		};
    		pins3 {
    			pinmux = <STM32_PINMUX('B', 11, AF11)>, /* ETH1_TX_CTL */
    					 <STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
    					 <STM32_PINMUX('C', 2, AF11)>, /* ETH1_TXD2 */
    					 <STM32_PINMUX('E', 2, AF11)>, /* ETH1_TXD3 */
    					 <STM32_PINMUX('G', 4, AF11)>, /* ETH1_GTX_CLK */
    					 <STM32_PINMUX('G', 5, AF11)>, /* ETH1_CLK125 */
    					 <STM32_PINMUX('G', 13, AF11)>, /* ETH1_TXD0 */
    					 <STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <2>;
    		};
    		pins4 {
    			pinmux = <STM32_PINMUX('B', 5, AF0)>; /* ETH1_CLK */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    	};
    
    	eth1_sleep_pins_mx: eth1_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 1, ANALOG)>, /* ETH1_RX_CLK */
    					 <STM32_PINMUX('A', 2, ANALOG)>, /* ETH1_MDIO */
    					 <STM32_PINMUX('A', 7, ANALOG)>, /* ETH1_RX_CTL */
    					 <STM32_PINMUX('B', 0, ANALOG)>, /* ETH1_RXD2 */
    					 <STM32_PINMUX('B', 5, ANALOG)>, /* ETH1_CLK */
    					 <STM32_PINMUX('B', 11, ANALOG)>, /* ETH1_TX_CTL */
    					 <STM32_PINMUX('C', 1, ANALOG)>, /* ETH1_MDC */
    					 <STM32_PINMUX('C', 2, ANALOG)>, /* ETH1_TXD2 */
    					 <STM32_PINMUX('C', 4, ANALOG)>, /* ETH1_RXD0 */
    					 <STM32_PINMUX('C', 5, ANALOG)>, /* ETH1_RXD1 */
    					 <STM32_PINMUX('E', 2, ANALOG)>, /* ETH1_TXD3 */
    					 <STM32_PINMUX('G', 4, ANALOG)>, /* ETH1_GTX_CLK */
    					 <STM32_PINMUX('G', 5, ANALOG)>, /* ETH1_CLK125 */
    					 <STM32_PINMUX('G', 13, ANALOG)>, /* ETH1_TXD0 */
    					 <STM32_PINMUX('G', 14, ANALOG)>, /* ETH1_TXD1 */
    					 <STM32_PINMUX('H', 7, ANALOG)>; /* ETH1_RXD3 */
    		};
    	};
    
    	hdmi_cec_pins_mx: hdmi_cec_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('B', 6, AF5)>; /* CEC */
    			bias-disable;
    			drive-open-drain;
    			slew-rate = <0>;
    		};
    	};
    
    	hdmi_cec_sleep_pins_mx: hdmi_cec_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('B', 6, ANALOG)>; /* CEC */
    		};
    	};
    
    	i2c1_pins_mx: i2c1_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('D', 12, AF5)>, /* I2C1_SCL */
    					 <STM32_PINMUX('D', 13, AF5)>; /* I2C1_SDA */
    			bias-disable;
    			drive-open-drain;
    			slew-rate = <0>;
    		};
    	};
    
    	i2c1_sleep_pins_mx: i2c1_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('D', 12, ANALOG)>, /* I2C1_SCL */
    					 <STM32_PINMUX('D', 13, ANALOG)>; /* I2C1_SDA */
    		};
    	};
    
    	i2c4_pins_mx: i2c4_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('F', 14, AF4)>, /* I2C4_SCL */
    					 <STM32_PINMUX('F', 15, AF4)>; /* I2C4_SDA */
    			bias-disable;
    			drive-open-drain;
    			slew-rate = <0>;
    		};
    	};
    
    	i2c4_sleep_pins_mx: i2c4_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('F', 14, ANALOG)>, /* I2C4_SCL */
    					 <STM32_PINMUX('F', 15, ANALOG)>; /* I2C4_SDA */
    		};
    	};
    
    	i2s2_pins_mx: i2s2_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 9, AF5)>, /* I2S2_CK */
    					 <STM32_PINMUX('B', 12, AF5)>, /* I2S2_WS */
    					 <STM32_PINMUX('I', 3, AF5)>; /* I2S2_SDO */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    	};
    
    	i2s2_sleep_pins_mx: i2s2_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 9, ANALOG)>, /* I2S2_CK */
    					 <STM32_PINMUX('B', 12, ANALOG)>, /* I2S2_WS */
    					 <STM32_PINMUX('I', 3, ANALOG)>; /* I2S2_SDO */
    		};
    	};
    
    	ltdc_pins_mx: ltdc_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('A', 3, AF14)>, /* LTDC_B5 */
    					 <STM32_PINMUX('B', 1, AF14)>, /* LTDC_G0 */
    					 <STM32_PINMUX('B', 8, AF14)>, /* LTDC_B6 */
    					 <STM32_PINMUX('C', 0, AF14)>, /* LTDC_R5 */
    					 <STM32_PINMUX('D', 8, AF14)>, /* LTDC_B7 */
    					 <STM32_PINMUX('D', 9, AF14)>, /* LTDC_B0 */
    					 <STM32_PINMUX('D', 10, AF14)>, /* LTDC_B3 */
    					 <STM32_PINMUX('E', 6, AF14)>, /* LTDC_G1 */
    					 <STM32_PINMUX('E', 15, AF14)>, /* LTDC_R7 */
    					 <STM32_PINMUX('F', 10, AF14)>, /* LTDC_DE */
    					 <STM32_PINMUX('G', 10, AF14)>, /* LTDC_B2 */
    					 <STM32_PINMUX('G', 12, AF14)>, /* LTDC_B1 */
    					 <STM32_PINMUX('H', 2, AF14)>, /* LTDC_R0 */
    					 <STM32_PINMUX('H', 3, AF14)>, /* LTDC_R1 */
    					 <STM32_PINMUX('H', 8, AF14)>, /* LTDC_R2 */
    					 <STM32_PINMUX('H', 9, AF14)>, /* LTDC_R3 */
    					 <STM32_PINMUX('H', 10, AF14)>, /* LTDC_R4 */
    					 <STM32_PINMUX('H', 12, AF14)>, /* LTDC_R6 */
    					 <STM32_PINMUX('H', 13, AF14)>, /* LTDC_G2 */
    					 <STM32_PINMUX('H', 14, AF14)>, /* LTDC_G3 */
    					 <STM32_PINMUX('H', 15, AF14)>, /* LTDC_G4 */
    					 <STM32_PINMUX('I', 0, AF14)>, /* LTDC_G5 */
    					 <STM32_PINMUX('I', 1, AF14)>, /* LTDC_G6 */
    					 <STM32_PINMUX('I', 2, AF14)>, /* LTDC_G7 */
    					 <STM32_PINMUX('I', 4, AF14)>, /* LTDC_B4 */
    					 <STM32_PINMUX('I', 9, AF14)>, /* LTDC_VSYNC */
    					 <STM32_PINMUX('I', 10, AF14)>; /* LTDC_HSYNC */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <0>;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('G', 7, AF14)>; /* LTDC_CLK */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    	};
    
    	ltdc_sleep_pins_mx: ltdc_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 3, ANALOG)>, /* LTDC_B5 */
    					 <STM32_PINMUX('B', 1, ANALOG)>, /* LTDC_G0 */
    					 <STM32_PINMUX('B', 8, ANALOG)>, /* LTDC_B6 */
    					 <STM32_PINMUX('C', 0, ANALOG)>, /* LTDC_R5 */
    					 <STM32_PINMUX('D', 8, ANALOG)>, /* LTDC_B7 */
    					 <STM32_PINMUX('D', 9, ANALOG)>, /* LTDC_B0 */
    					 <STM32_PINMUX('D', 10, ANALOG)>, /* LTDC_B3 */
    					 <STM32_PINMUX('E', 6, ANALOG)>, /* LTDC_G1 */
    					 <STM32_PINMUX('E', 15, ANALOG)>, /* LTDC_R7 */
    					 <STM32_PINMUX('F', 10, ANALOG)>, /* LTDC_DE */
    					 <STM32_PINMUX('G', 7, ANALOG)>, /* LTDC_CLK */
    					 <STM32_PINMUX('G', 10, ANALOG)>, /* LTDC_B2 */
    					 <STM32_PINMUX('G', 12, ANALOG)>, /* LTDC_B1 */
    					 <STM32_PINMUX('H', 2, ANALOG)>, /* LTDC_R0 */
    					 <STM32_PINMUX('H', 3, ANALOG)>, /* LTDC_R1 */
    					 <STM32_PINMUX('H', 8, ANALOG)>, /* LTDC_R2 */
    					 <STM32_PINMUX('H', 9, ANALOG)>, /* LTDC_R3 */
    					 <STM32_PINMUX('H', 10, ANALOG)>, /* LTDC_R4 */
    					 <STM32_PINMUX('H', 12, ANALOG)>, /* LTDC_R6 */
    					 <STM32_PINMUX('H', 13, ANALOG)>, /* LTDC_G2 */
    					 <STM32_PINMUX('H', 14, ANALOG)>, /* LTDC_G3 */
    					 <STM32_PINMUX('H', 15, ANALOG)>, /* LTDC_G4 */
    					 <STM32_PINMUX('I', 0, ANALOG)>, /* LTDC_G5 */
    					 <STM32_PINMUX('I', 1, ANALOG)>, /* LTDC_G6 */
    					 <STM32_PINMUX('I', 2, ANALOG)>, /* LTDC_G7 */
    					 <STM32_PINMUX('I', 4, ANALOG)>, /* LTDC_B4 */
    					 <STM32_PINMUX('I', 9, ANALOG)>, /* LTDC_VSYNC */
    					 <STM32_PINMUX('I', 10, ANALOG)>; /* LTDC_HSYNC */
    		};
    	};
    
    	sdmmc2_pins_mx: sdmmc2_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
    					 <STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
    					 <STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
    					 <STM32_PINMUX('B', 9, AF10)>, /* SDMMC2_D5 */
    					 <STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
    					 <STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
    					 <STM32_PINMUX('E', 5, AF9)>; /* SDMMC2_D6 */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
    					 <STM32_PINMUX('E', 3, AF9)>, /* SDMMC2_CK */
    					 <STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
    			bias-pull-up;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    	};
    
    	sdmmc2_opendrain_pins_mx: sdmmc2_opendrain_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
    					 <STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
    					 <STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
    					 <STM32_PINMUX('B', 9, AF10)>, /* SDMMC2_D5 */
    					 <STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
    					 <STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
    					 <STM32_PINMUX('E', 5, AF9)>; /* SDMMC2_D6 */
    			bias-disable;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
    					 <STM32_PINMUX('E', 3, AF9)>; /* SDMMC2_CK */
    			bias-pull-up;
    			drive-push-pull;
    			slew-rate = <1>;
    		};
    		pins3 {
    			pinmux = <STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
    			bias-pull-up;
    			drive-open-drain;
    			slew-rate = <1>;
    		};
    	};
    
    	sdmmc2_sleep_pins_mx: sdmmc2_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 8, ANALOG)>, /* SDMMC2_D4 */
    					 <STM32_PINMUX('B', 3, ANALOG)>, /* SDMMC2_D2 */
    					 <STM32_PINMUX('B', 4, ANALOG)>, /* SDMMC2_D3 */
    					 <STM32_PINMUX('B', 9, ANALOG)>, /* SDMMC2_D5 */
    					 <STM32_PINMUX('B', 14, ANALOG)>, /* SDMMC2_D0 */
    					 <STM32_PINMUX('B', 15, ANALOG)>, /* SDMMC2_D1 */
    					 <STM32_PINMUX('C', 7, ANALOG)>, /* SDMMC2_D7 */
    					 <STM32_PINMUX('E', 3, ANALOG)>, /* SDMMC2_CK */
    					 <STM32_PINMUX('E', 5, ANALOG)>, /* SDMMC2_D6 */
    					 <STM32_PINMUX('G', 6, ANALOG)>; /* SDMMC2_CMD */
    		};
    	};
    
    	uart4_pins_mx: uart4_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */
    			bias-pull-up;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('G', 11, AF6)>; /* UART4_TX */
    			bias-pull-up;
    			drive-push-pull;
    			slew-rate = <0>;
    		};
    	};
    
    	uart4_idle_pins_mx: uart4_idle_mx-0 {
    		pins1 {
    			pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */
    			bias-pull-up;
    		};
    		pins2 {
    			pinmux = <STM32_PINMUX('G', 11, ANALOG)>; /* UART4_TX */
    			bias-pull-up;
    		};
    	};
    
    	uart4_sleep_pins_mx: uart4_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('B', 2, ANALOG)>, /* UART4_RX */
    					 <STM32_PINMUX('G', 11, ANALOG)>; /* UART4_TX */
    			bias-pull-up;
    		};
    	};
    
    	usb_otg_hs_pins_mx: usb_otg_hs_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 10, ANALOG)>; /* USB_OTG_HS_ID */
    		};
    	};
    
    	usb_otg_hs_sleep_pins_mx: usb_otg_hs_sleep_mx-0 {
    		pins {
    			pinmux = <STM32_PINMUX('A', 10, ANALOG)>; /* USB_OTG_HS_ID */
    		};
    	};
    
    	/* USER CODE BEGIN pinctrl */
    	/* USER CODE END pinctrl */
    };
    
    &pinctrl_z {
    
    	/* USER CODE BEGIN pinctrl_z */
    	/* USER CODE END pinctrl_z */
    };
    
    &m4_rproc{
    	status = "disabled";
    
    	/* USER CODE BEGIN m4_rproc */
    	resets = <&scmi_reset RST_SCMI_MCU>, <&scmi_reset RST_SCMI_MCU_HOLD_BOOT>;
    	reset-names = "mcu_rst", "hold_boot";
    	/*/delete-property/ st,syscfg-holdboot;*/
    	mboxes = <&ipcc 0>, <&ipcc 1>, <&ipcc 2>, <&ipcc 3>;
    	mbox-names = "vq0", "vq1", "shutdown", "detach";
    	memory-region = <&retram>, <&mcuram>, <&mcuram2>, <&vdev0vring0>, <&vdev0vring1>, <&vdev0buffer>, <&mcu_rsc_table>;
    	interrupt-parent = <&exti>;
    	interrupts = <68 1>;
    	wakeup-source;
    	/* USER CODE END m4_rproc */
    
    	m4_system_resources{
    		status = "disabled";
    
    		/* USER CODE BEGIN m4_system_resources */
    		/* USER CODE END m4_system_resources */
    	};
    };
    
    &bsec{
    	status = "okay";
    
    	/* USER CODE BEGIN bsec */
    	/* USER CODE END bsec */
    };
    
    &cec{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&hdmi_cec_pins_mx>;
    	pinctrl-1 = <&hdmi_cec_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN cec */
    	/* USER CODE END cec */
    };
    
    &dma1{
    	status = "okay";
    
    	/* USER CODE BEGIN dma1 */
    	resets = <&scmi_reset RST_SCMI_MDMA>;
    	/* USER CODE END dma1 */
    };
    
    &dma2{
    	status = "disabled";
    
    	/* USER CODE BEGIN dma2 */
    	/* USER CODE END dma2 */
    };
    
    &dmamux1{
    	status = "okay";
    
    	dma-masters = <&dma1>;
    	dma-channels = <8>;
    
    	/* USER CODE BEGIN dmamux1 */
    	/* USER CODE END dmamux1 */
    };
    
    &ethernet0{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&eth1_pins_mx>;
    	pinctrl-1 = <&eth1_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN ethernet0 */
    	phy-mode = "rgmii-id";
    	max-speed = <1000>;
    	phy-handle = <&phy0>;
    	nvmem-cells = <&ethernet_mac_address>;
    	nvmem-cell-names = "mac-address";
    
    	mdio{
    		#address-cells = <1>;
    		#size-cells = <0>;
    		compatible = "snps,dwmac-mdio";
    
    		phy0:ethernet-phy@0{
    			reg = <0>;
    		};
    	};
    	/* USER CODE END ethernet0 */
    };
    
    &hsem{
    	status = "okay";
    
    	/* USER CODE BEGIN hsem */
    	/* USER CODE END hsem */
    };
    
    &i2c1{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&i2c1_pins_mx>;
    	pinctrl-1 = <&i2c1_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN i2c1 */
    	/* USER CODE END i2c1 */
    };
    
    &i2c4{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&i2c4_pins_mx>;
    	pinctrl-1 = <&i2c4_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN i2c4 */
    	clocks = <&scmi_clk CK_SCMI_I2C4>;
    	resets = <&scmi_reset RST_SCMI_I2C4>;
    	i2c-scl-rising-time-ns = <185>;
    	i2c-scl-falling-time-ns = <20>;
    	clock-frequency = <400000>;
    	/delete-property/ dmas;
    	/delete-property/ dma-names;
    
    	sii9022A: hdmi-transmitter@39{
    		compatible = "sil,sii9022";
    		reg = <0x39>;
    		iovcc-supply = <&v3v3_hdmi>;
    		cvcc12-supply = <&v1v2_hdmi>;
    		reset-gpios = <&gpioe 8 GPIO_ACTIVE_LOW>;
    		interrupts = <1 IRQ_TYPE_EDGE_FALLING>;
    		interrupt-parent = <&gpiog>;
    		#sound-dai-cells = <0>;
    		sil,i2s-data-lanes = <0>;
    		/*clocks = <&mclk>;
    		clock-names = "mclk";*/
    		status = "okay";
    
    		ports{
    			#address-cells = <1>;
    			#size-cells = <0>;
    
    			port@0{
    				reg = <0>;
    
    				sii9022_in:endpoint{
    					remote-endpoint = <&ltdc_ep0_out>;
    				};
    			};
    
    			port@1{
    				reg = <1>;
    
    				sii9022_out:endpoint{
    					remote-endpoint = <&hdmi_connector_in>;
    				};
    			};
    
    			port@3{
    				reg = <3>;
    
    				sii9022_tx_endpoint:endpoint{
    					remote-endpoint = <&i2s2_endpoint>;
    				};
    			};
    		};
    	};
    	
    	pmic:stpmic@33{
    		compatible = "st,stpmic1";
    		reg = <0x33>;
    		/*interrupts-extended = <&gpioa 0 IRQ_TYPE_EDGE_FALLING>;*/
    		interrupts-extended = <&exti 55 IRQ_TYPE_EDGE_FALLING>;
    		interrupt-controller;
    		#interrupt-cells = <2>;
    		status = "okay";
    
    		regulators{
    			compatible = "st,stpmic1-regulators";
    			buck1-supply = <&vin>;
    			buck2-supply = <&vin>;
    			buck3-supply = <&vin>;
    			buck4-supply = <&vin>;
    			/*ldo1-supply = <&v3v3>;*/
    			ldo2-supply = <&vin>;
    			ldo3-supply = <&vdd_ddr>;
    			ldo4-supply = <&vin>;
    			ldo5-supply = <&vin>;
    			ldo6-supply = <&v3v3>;
    			vref_ddr-supply = <&vin>;
    			/*boost-supply = <&vin>;
    			pwr_sw1-supply = <&bst_out>;
    			pwr_sw2-supply = <&bst_out>;*/
    
    			vddcore:buck1{
    				regulator-name = "vddcore";
    				regulator-min-microvolt = <1200000>;
    				regulator-max-microvolt = <1350000>;
    				regulator-always-on;
    				regulator-initial-mode = <0>;
    				regulator-over-current-protection;
    			};
    
    			vdd_ddr:buck2{
    				regulator-name = "vdd_ddr";
    				regulator-min-microvolt = <1350000>;
    				regulator-max-microvolt = <1350000>;
    				regulator-always-on;
    				regulator-initial-mode = <0>;
    				regulator-over-current-protection;
    			};
    
    			vdd:buck3{
    				regulator-name = "vdd";
    				regulator-min-microvolt = <3300000>;
    				regulator-max-microvolt = <3300000>;
    				regulator-always-on;
    				st,mask-reset;
    				regulator-initial-mode = <0>;
    				regulator-over-current-protection;
    			};
    
    			v3v3:buck4{
    				regulator-name = "v3v3";
    				regulator-min-microvolt = <3300000>;
    				regulator-max-microvolt = <3300000>;
    				regulator-always-on;
    				regulator-over-current-protection;
    				regulator-initial-mode = <0>;
    			};
    			
    			/*
    			v1v8_audio:ldo1{
    				regulator-name = "v1v8_audio";
    				regulator-min-microvolt = <1800000>;
    				regulator-max-microvolt = <1800000>;
    				regulator-always-on;
    				interrupts = <IT_CURLIM_LDO1 0>;
    			};*/
    
    			v3v3_hdmi:ldo2{
    				regulator-name = "v3v3_hdmi";
    				regulator-min-microvolt = <3300000>;
    				regulator-max-microvolt = <3300000>;
    				regulator-always-on;
    				interrupts = <IT_CURLIM_LDO2 0>;
    			};
    
    			vtt_ddr:ldo3{
    				regulator-name = "vtt_ddr";
    				regulator-min-microvolt = <500000>;
    				regulator-max-microvolt = <750000>;
    				regulator-always-on;
    				regulator-over-current-protection;
    			};
    
    			vdd_usb:ldo4{
    				regulator-name = "vdd_usb";
    				interrupts = <IT_CURLIM_LDO4 0>;
    			};
    
    			vdda:ldo5{
    				regulator-name = "vdda";
    				regulator-min-microvolt = <2900000>;
    				regulator-max-microvolt = <2900000>;
    				interrupts = <IT_CURLIM_LDO5 0>;
    				regulator-boot-on;
    			};
    
    			v1v2_hdmi:ldo6{
    				regulator-name = "v1v2_hdmi";
    				regulator-min-microvolt = <1200000>;
    				regulator-max-microvolt = <1200000>;
    				regulator-always-on;
    				interrupts = <IT_CURLIM_LDO6 0>;
    			};
    
    			vref_ddr:vref-ddr{
    				regulator-name = "vref_ddr";
    				regulator-always-on;
    			};
    
    			/*
    			bst_out:boost{
    				regulator-name = "bst_out";
    				interrupts = <IT_OCP_BOOST 0>;
    			};
    
    			vbus_otg:pwr-sw1{
    				regulator-name = "vbus_otg";
    				interrupts = <IT_OCP_OTG 0>;
    			};
    
    			vbus_sw:pwr-sw2{
    				regulator-name = "vbus_sw";
    				interrupts = <IT_OCP_SWOUT 0>;
    				regulator-active-discharge = <1>;
    			};
    			*/
    		};
    
    		onkey{
    			compatible = "st,stpmic1-onkey";
    			interrupts = <IT_PONKEY_F 0>, <IT_PONKEY_R 0>;
    			interrupt-names = "onkey-falling", "onkey-rising";
    			power-off-time-sec = <10>;
    			status = "okay";
    		};
    	};
    	/* USER CODE END i2c4 */
    };
    
    &i2s2{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&i2s2_pins_mx>;
    	pinctrl-1 = <&i2s2_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN i2s2 */
    	clocks = <&rcc SPI2>, <&rcc SPI2_K>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
    	clock-names = "pclk", "i2sclk", "x8k", "x11k";
    
    	i2s2_port:port{
    		i2s2_endpoint:endpoint{
    			remote-endpoint = <&sii9022_tx_endpoint>;
    			dai-format = "i2s";
    			mclk-fs = <256>;
    		};
    	};
    	/* USER CODE END i2s2 */
    };
    
    &ltdc{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&ltdc_pins_mx>;
    	pinctrl-1 = <&ltdc_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN ltdc */
    	port{
    
    		ltdc_ep0_out:endpoint{
    			remote-endpoint = <&sii9022_in>;
    		};
    	};
    	/* USER CODE END ltdc */
    };
    
    &m4_dma2{
    	status = "okay";
    
    	/* USER CODE BEGIN m4_dma2 */
    	/* USER CODE END m4_dma2 */
    };
    
    &mdma1{
    	status = "okay";
    
    	/* USER CODE BEGIN mdma1 */
    	/* USER CODE END mdma1 */
    };
    
    &pwr_regulators{
    	status = "okay";
    
    	/* USER CODE BEGIN pwr_regulators */
    	vdd-supply = <&vdd>;
    	vdd_3v3_usbfs-supply = <&vdd_usb>;
    	/* USER CODE END pwr_regulators */
    };
    
    &rcc{
    	status = "okay";
    
    	/* USER CODE BEGIN rcc */
    	compatible = "st,stm32mp1-rcc-secure", "syscon";
    	clock-names = "hse", "hsi", "csi", "lse", "lsi";
    	clocks = <&scmi_clk CK_SCMI_HSE>,
    		 <&scmi_clk CK_SCMI_HSI>,
    		 <&scmi_clk CK_SCMI_CSI>,
    		 <&scmi_clk CK_SCMI_LSE>,
    		 <&scmi_clk CK_SCMI_LSI>;
    	/* USER CODE END rcc */
    };
    
    &rng1{
    	status = "okay";
    
    	/* USER CODE BEGIN rng1 */
    	clocks = <&scmi_clk CK_SCMI_RNG1>;
    	resets = <&scmi_reset RST_SCMI_RNG1>;
    	/* USER CODE END rng1 */
    };
    
    &rtc{
    	status = "okay";
    
    	/* USER CODE BEGIN rtc */
    	clocks = <&scmi_clk CK_SCMI_RTCAPB>, <&scmi_clk CK_SCMI_RTC>;
    	/* USER CODE END rtc */
    };
    
    &sdmmc2{
    	pinctrl-names = "default", "opendrain", "sleep";
    	pinctrl-0 = <&sdmmc2_pins_mx>;
    	pinctrl-1 = <&sdmmc2_opendrain_pins_mx>;
    	pinctrl-2 = <&sdmmc2_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN sdmmc2 */
    	non-removable;
    	no-sd;
    	no-sdio;
    	st,neg-edge;
    	bus-width = <8>;
    	vmmc-supply = <&v3v3>;
    	vqmmc-supply = <&vdd>;
    	mmc-ddr-3_3v;
    	/* USER CODE END sdmmc2 */
    };
    
    &tamp{
    	status = "okay";
    
    	/* USER CODE BEGIN tamp */
    	/* USER CODE END tamp */
    };
    
    &uart4{
    	pinctrl-names = "default", "idle", "sleep";
    	pinctrl-0 = <&uart4_pins_mx>;
    	pinctrl-1 = <&uart4_idle_pins_mx>;
    	pinctrl-2 = <&uart4_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN uart4 */
    	/delete-property/ dmas;
    	/delete-property/ dma-names;
    	u-boot,dm-pre-reloc;
    	/* USER CODE END uart4 */
    };
    
    &usbh_ehci{
    	status = "okay";
    
    	/* USER CODE BEGIN usbh_ehci */
    	phys = <&usbphyc_port0>;
    	#address-cells = <1>;
    	#size-cells = <0>;
    	/* onboard HUB */
    	hub@1 {
    		compatible = "usb424,2514";
    		reg = <1>;
    		vdd-supply = <&v3v3>;
    	};
    	/* USER CODE END usbh_ehci */
    };
    
    &usbh_ohci{
    	status = "okay";
    
    	/* USER CODE BEGIN usbh_ohci */
    	/* USER CODE END usbh_ohci */
    };
    
    &usbotg_hs{
    	pinctrl-names = "default", "sleep";
    	pinctrl-0 = <&usb_otg_hs_pins_mx>;
    	pinctrl-1 = <&usb_otg_hs_sleep_pins_mx>;
    	status = "okay";
    
    	/* USER CODE BEGIN usbotg_hs */
    	phys = <&usbphyc_port1 0>;
    	phy-names = "usb2-phy";
    	usb-role-switch;
     u-boot,dm-pre-reloc; 
     u-boot,force-b-session-valid;
     hnp-srp-disable;
     dr_mode = "peripheral"; 
    	/* USER CODE END usbotg_hs */
    };
    
    &usbphyc{
    	status = "okay";
    
    	/* USER CODE BEGIN usbphyc */
    	phy-supply = <&vdd_usb>;
    	/* USER CODE END usbphyc */
    };
    
    &usbphyc_port0{
    	status = "okay";
    
    	/* USER CODE BEGIN usbphyc_port0 */
    	phy-supply = <&vdd_usb>;
    	st,tune-hs-dc-level = <2>;
    	st,enable-fs-rftime-tuning;
    	st,enable-hs-rftime-reduction;
    	st,trim-hs-current = <15>;
    	st,trim-hs-impedance = <1>;
    	st,tune-squelch-level = <3>;
    	st,tune-hs-rx-offset = <2>;
    	st,no-lsfs-sc;
    	/* USER CODE END usbphyc_port0 */
    };
    
    &usbphyc_port1{
    	status = "okay";
    
    	/* USER CODE BEGIN usbphyc_port1 */
    	phy-supply = <&vdd_usb>;
    	st,tune-hs-dc-level = <2>;
    	st,enable-fs-rftime-tuning;
    	st,enable-hs-rftime-reduction;
    	st,trim-hs-current = <15>;
    	st,trim-hs-impedance = <1>;
    	st,tune-squelch-level = <3>;
    	st,tune-hs-rx-offset = <2>;
    	st,no-lsfs-sc;
    	/* USER CODE END usbphyc_port1 */
    };
    
    /* USER CODE BEGIN addons */
    /*
    &arm_wdt{
    	timeout-sec = <32>;
    	status = "okay";
    };
    */
    &cpu0 {
    	cpu-supply = <&vddcore>;
    	clocks = <&scmi_clk CK_SCMI_MPU>;
    };
    
    &uart4_pins_mx {
    	u-boot,dm-pre-reloc;
    	pins1 {
    		u-boot,dm-pre-reloc;
    	};
    	pins2 {
    		u-boot,dm-pre-reloc;
    	};
    };
    &gpioz {
    	clocks = <&scmi_clk CK_SCMI_GPIOZ>;
    };
    /* USER CODE END addons */