Skip to main content
Visitor II
November 9, 2022
Solved

Can we use W634GU6NB-11 (Winbond Speed grade 1866) with STM32MP1ADD3 ?

  • November 9, 2022
  • 1 reply
  • 1410 views

Hi,

 

Can we use a DDR3L from Winbond with part number W634GU6NB-11 (Speed bin 1866) with STMPU STM32MP1ADD3.

As STM32MP1 datasheet suggest that it can support up-to 1066. So using above part from Winbond will have any interface issue ?

 

Thanks.

 

Hi @Community member​ 

can you please share your input on above issue.

 

    This topic has been closed for replies.
    Best answer by PatrickF

    Hi @PS.2​ 

    Faster memory could work at slower frequency.

    Will likely work with default DDR3L-1066 conservative settings. Please look at AN5168 for details of configuration choices which could probably enhance a bit the performances (CL improvement gain is usually barely noticeable at system level, especially on x32 DDR).

    Regards.

    1 reply

    PatrickFAnswer
    Technical Moderator
    November 9, 2022

    Hi @PS.2​ 

    Faster memory could work at slower frequency.

    Will likely work with default DDR3L-1066 conservative settings. Please look at AN5168 for details of configuration choices which could probably enhance a bit the performances (CL improvement gain is usually barely noticeable at system level, especially on x32 DDR).

    Regards.