Cannot access LPDDR3 memory from a STM32MP153AABxx
Hi,
on a custom board with a STM32MP153AABxx and a W63AH6NBV 1Gbit LPDDR3 memory I am failing to initialise the DDR properly. I made the required changes to the upstream u-boot device tree files, added support for UART8 debug console and some minor things and compiled the SPL. I enabled the DDR interactive console and loaded SPL to the MPU using STM32 cube programmer CLI. STPMIC1 is properly configured, 1V2 and 1V8 DDR power rails are present. So far, so good. Trying DDR tests one-by-one, all are failing.
LPDDR3 is wired according to AN5031 (Rev 4), section 10.1.7. I tried ODT both grounded and connected to the MPU. Routing should be OK.
In addition to this, I tried to use CubeMX DDR Test Suite. Having a running SPL I managed to connect to it. The tool correctly recognises the DDR as:
Config name: LPDDR3 16bits 533000kHz
DDR Size: 1 GBits
DDR Frequency: 533.0MHzThen it stops cooperating with:
Exception in thread "Thread-4843" java.lang.ArrayIndexOutOfBoundsException: Index 1 out of bounds for length 1I will appreciate any ideas.