Cannot generate TIM5 global interrupt in STM32MP151
I use STM32MP151CAA3 mounted on my own board.
I want to generate TIM5 global interrupt in Cortex-M4.
I have written following code, However, TIM5 global interrupt doesn't occurs (TIM5_IRQHandler doesn't be called).
In Keil MDK-ARM Debbuger, I have confirmed following settings are reflected.
--TIM5_DIER->UIE = 1
--TIM5_CR1->CEN = 1
--When TIM5 CNT reach TIM5_ARR value, TIM5_SR->UIF is set.
#include "stm32mp1xx_hal.h"
void TIM5_Start(void)
{
TIM_HandleTypeDef m_handleTim5;
TIM_ClockConfigTypeDef sClockSourceConfig;
TIM_MasterConfigTypeDef sMasterConfig;
__HAL_RCC_TIM5_CLK_ENABLE();
m_handleTim5.Instance = TIM5;
m_handleTim5.Init.Prescaler = 41999;
m_handleTim5.Init.CounterMode = TIM_COUNTERMODE_UP;
m_handleTim5.Init.Period = 0;
m_handleTim5.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
HAL_TIM_Base_Init(&m_handleTim5);
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
HAL_TIM_ConfigClockSource(&m_handleTim5, &sClockSourceConfig);
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
HAL_TIMEx_MasterConfigSynchronization(&m_handleTim5, &sMasterConfig);
HAL_NVIC_EnableIRQ(TIM5_IRQn);
TIM5->ARR = (time * 2) - 1;
TIM5->EGR |= TIM_EGR_UG;
TIM5->SR = 0;
HAL_TIM_Base_Start_IT(&m_handleTim5);
}For your reference, TIM4 global interrupt does not occurs similarly.
But TIM6 or TIM7 global interrupt occurs without any problems.
Is there any missing in above code?
Best Regards.
H. Masuda