Cannot light up the LCD of STM32MPU135-DK
- If the board power supply does not supply enough current (3A), the red LED indicates the issue following the rules below:
LED blinking mode Console message Boot process
| Twice | WARNING 500mA power supply detected Current too low, use a 3A power supply! | Continue and red LED stays ON |
| 3 times | WARNING 1500mA power supply detected Current too low, use a 3A power supply! | Continue and red LED stays ON |
| forever | ERROR USB TYPE-C connection in unattached mode Check that USB TYPE-C cable is correctly plugged | stop |
| forever | USB TYPE-C charger not compliant with USB specification | stop |
I confirm that my power supply supports 5V3A.
my log as follow:
Previous ADC measurements was not the one expected, retry in 20ms
********************************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
*******************************************************