check host USB0 cfg
STM32WB version 2.9.1.2019050314
Linux version 4.15.0.72 64b
Eclipse version Neon.3 release 4.6.3
Java version 11.0.5 2019-10-15
Distro Linux Mint 19.2 Tina
I am using the discovery stm32mp1-157 and trying to follow the wiki tutorial. I have been able to build the is and load it and reboot. I have been successful in creating the gtk hello world, loading it to the board and running it. Now I am trying to do the OpenAMP_TTY_echo project. It compiles fine but when I try to start the debugger the connection fails indicating “Ethernet over usb0 connection�? error. The target widget in the lower right corner cycles through Status:idle, Device: /dev/ttyACM0, Addr: 192.168.7.2, check host usb0 cfg!.
Has anyone else run into this?
I have tried to fix it by adding group permissions for dial out and try to user name but no change.
I suspect a permissions problem but cannot figure it out.
I also checked the board side using the serial connection in SWB4STM and verified That the eth address for the board is 192.168.7.2.
The serial connection is not active while trying to use the debugger.