Compatibility with Audio Injector and Cortex M4 usage on STM32MP157D-DK1
Hi,
We have acquired this board called Audio Injector (in the image) that has a WM8731, it is a raspberry pi hat, but we want to use it with the STM32MP157D-DK1 but the drivers we have found on the internet seems to be not compatible with this board (we are using the base OpenSTLinux), despite the board has the pinout of raspberry. Someone has used it before?
Another question, how can we manipulate the Cortex M4 from the Operating system? there is a way we can use it capabilities from the OS? because we noticed that for the Cortex A7 we cannot use the SAI ports as I2S but from the Cortex M4 is possible to use them as I2S. (we saw that on the STM32Cube IDE and CubeMX).
Thanks for your answer.