Connecting USB to Cortex-M4 on STM32mp157 possible?
I'd like to connect one USB port to the RTOS, running on the Cortex-M4. According CubeMX this is not possible (no square availble to tick). Is this really not possible?
According the datasheet (DS12505 Rev3, page 19, 'Block Diagram'):
- USBH is connected to AXIM bus, but the corresponding arrow is blue (= AHB ).
- The USB OTG I can not find there.
According same datasheet (page 36, 'Bus Matirx'):
- USBH is connected to AXIM
- USBO is connected to MLAHB
This is not clear to me.
Denise