Custom board openstlinux distribution problem
Hi there,
I am building custom board with openstlinux distribution package with following config
Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-ostl-linux-gnueabi"
MACHINE = "stm32mp1-silico"
DISTRO = "openstlinux-weston"
DISTRO_VERSION = "4.0.4-snapshot-20230428"
TUNE_FEATURES = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"
TARGET_FPU = "hard"
DISTRO_CODENAME = "kirkstone"
ACCEPT_EULA_stm32mp1-silico = "1"
GCCVERSION = "11.%"
PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"
It all goes splendidly and board boots up with following log.
2.663121] EXT4-fs (mmcblk1p10): recovery complete
[ 2.724133] EXT4-fs (mmcblk1p10): mounted filesystem with ordered data mode. Opts: (null). Quota mode: disabled.
[ 2.733150] VFS: Mounted root (ext4 filesystem) on device 179:10.
[ 2.740392] devtmpfs: mounted
[ 2.745412] Freeing unused kernel image (initmem) memory: 1024K
[ 2.750736] Run /sbin/init as init process
[ 2.759550] Run /etc/init as init process
[ 2.763368] Run /bin/init as init process
[ 2.768285] Run /bin/sh as init process
/bin/sh: can't access tty; job control turned off
/ #
I've expected it use systemd as init process but it seems to be using /bin/sh. Thing is there is no
sbin/init (nor /etc/init for that matter) in rootfs. The system is configured to use systemd as init
bitbake-getvar VIRTUAL-RUNTIME_init_manager shows
# $VIRTUAL-RUNTIME_init_manager [2 operations]
# set /home/redacted/Projects/openstlinuxdist-silico/layers/meta-st/meta-st-openstlinux/conf/distro/include/openstlinux.inc:89
# "systemd"
# set /home/redacted/Projects/openstlinuxdist-silico/layers/openembedded-core/meta/conf/distro/include/init-manager-none.inc:1
# [_defaultval] "sysvinit"
# pre-expansion value:
# "systemd"
VIRTUAL-RUNTIME_init_manager="systemd"
Setting it in local.conf didn't help either. systemd is also appears in
DISTRO_FEATURES.
Is there anything I might be missing?
Thanks in advance