DCMI resolution on STM32MP157c ?
I'm trying to use an ADV7280 videodecoder with DCMI and embedded linux on a board based on STM32157c-dk2. The decoder should output 720x576 picture resolution with the camera (PAL,CV) attached. However the DCMI seems to be in 'normal mode' which allows max 480x272 resolution based on app. note AN5020. How to change mode to circular buffer mode which should allow higher resolutions? I haven't found any linux device tree setups for that. Some settings for dma or dcmi ? Examples?