Skip to main content
Visitor II
July 14, 2023
Question

DDR Test suite binary file can not start

  • July 14, 2023
  • 0 replies
  • 1024 views

Try to conduct the DDR test to my STM32MP135 customized board,  following the instruction in the DDR test util:

https://github.com/STMicroelectronics/STM32DDRFW-UTIL

while after successfully download the test binary file, the test code didn't start,  I am using serial only for this test (not usb + uart),  seems the parameter  –-start 0x01 not accepted,  anyone has an idea of what is going on with it?

following is the full log:

xx@ubuntu:~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin$ ./STM32_Programmer_CLI -c port=ttyUSB0 -w STM32MP135C-DK_DDR_UTILITIES_A7_signed.stm32 0x01 –-start 0x01
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------

Serial Port ttyUSB0 is successfully opened.
Port configuration: parity = even, baudrate = 115200, data-bit = 8,
stop-bit = 1.0, flow-control = off
Activating device: OK
Board : --
Chip ID: 0x501
BootLoader protocol version: 4.0
Device name : STM32MP13xx
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7


Memory Programming ...
Opening and parsing file: STM32MP135C-DK_DDR_UTILITIES_A7_signed.stm32
File : STM32MP135C-DK_DDR_UTILITIES_A7_signed.stm32
Size : 54.50 KB
Partition ID : 0x01

Download in Progress:
[==================================================] 100%

File download complete
Time elapsed during download operation: 00:00:07.633
xx@ubuntu:~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin$

    This topic has been closed for replies.