Skip to main content
Visitor II
October 17, 2024
Question

Debug-Error on a STM32 Board - Error in final launch sequence

  • October 17, 2024
  • 3 replies
  • 3460 views

Hello Community,

we're trying to debug an STM32 image (kernel-version V6.1.28) on the M4 core using STLINK-V3SET debugger via STM32CubeIDE (V1.16.0) and getting the following error:

Error in final launch sequence: Failed pre launch (s. attached screenshot).

The directory /lib/firmware has space and is writeable.

Does anyone have an idea what the problem is?

The content of our local.conf:

MACHINE ??= 'txmp-1571'
DL_DIR ?= "${BSPDIR}/downloads"
SSTATE_DIR ?= "${BSPDIR}/sstate-cache"
DISTRO ?= 'karo-wayland'
DISTRO_FEATURES:append = " alternatives-symlinks-relative"
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES ?= "debug-tweaks"
USER_CLASSES ?= "buildstats"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS ??= "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
HALT,${TMPDIR},100M,1K \
HALT,${DL_DIR},100M,1K \
HALT,${SSTATE_DIR},100M,1K \
HALT,/tmp,10M,1K"
SSTATE_MIRRORS ?= "\
file://.* http://sstate.karo-electronics.de/PATH;downloadfilename=PATH \
"
PACKAGECONFIG:append:pn-qemu-native = " sdl"
PACKAGECONFIG:append:pn-nativesdk-qemu = " sdl"
CONF_VERSION = "2"
BB_HASHSERVE = ""
BB_SIGNATURE_HANDLER = "OEBasicHash"
VIRTUAL-RUNTIME_dev_manager ??= "udev"
ROOT_HOME = "/root"
SANITY_TESTED_DISTROS:append = " devuan-4"
unset SOURCE_DATE_EPOCH
REPRODUCIBLE_TIMESTAMP_ROOTFS = ""
KERNEL_DEBUG_TIMESTAMPS = "1"
DEFAULT_TIMEZONE = "Europe/Berlin"
IMAGE_INSTALL:append = " psplash nano openssh-sftp-server"

 

    This topic has been closed for replies.

    3 replies

    Graduate
    October 18, 2024

    Hi there,

    I maybe have the same issue. I try to debug the M4 core of a STM32MP157. I'm using the latest CubeIDE under Windows 10 LTS. I was able to debug the older Kernel 5.x images. The 6.x Kernel doesn't work at all.

    I can debug my FreeRTOS devices (STM32H7 and F7) without any issues.

    Visitor II
    October 23, 2024

    create the folder /lib/firmware by hand. STM32CubeIDE obviously expects it in the file system and is not able to create it by itself if it is not available.

    BuGeAuthor
    Visitor II
    October 24, 2024

    When I create this folder manually I get the new error: "Failed to execute MI command":

     

    BuGe_0-1729774030948.png

     

     

     

    Visitor II
    October 29, 2024

    it seems that the openocd server cannot be started correctly. The console output shows:

    Open On-Chip Debugger 0.12.0+dev-00597-ga5a21219f (2024-06-03-11:02) [https://github.com/STMicroelectronics/OpenOCD]
    Licensed under GNU GPL v2
    For bug reports, read
    srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
    Info : Listening on port 6666 for tcl connections
    Info : Listening on port 4444 for telnet connections
    Info : STLINK V3J15M7B5S1 (API v3) VID:PID 0483:374F
    Info : Target voltage: 3.287302
    Error: init mode failed (unable to connect to the target)
     
    when I add the -d option into the command line, it shows that it fails caused by an USB error:
     
    Open On-Chip Debugger 0.12.0+dev-00597-ga5a21219f (2024-06-03-11:02) [https://github.com/STMicroelectronics/OpenOCD]
    Licensed under GNU GPL v2
    For bug reports, read
    http://openocd.org/doc/doxygen/bugs.html
     
     
    ...



    Debug: 237 6 stlink_usb.c:5155 stlink_dap_init(): stlink_dap_init()
    Debug: 238 6 stlink_usb.c:3732 stlink_open(): stlink_open
    Debug: 239 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x3748 serial:
    Debug: 240 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x374b serial:
    Debug: 241 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x374d serial:
    Debug: 242 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x374e serial:
    Debug: 243 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x374f serial:
    Debug: 244 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x3752 serial:
    Debug: 245 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x3753 serial:
    Debug: 246 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x3754 serial:
    Debug: 247 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x3755 serial:
    Debug: 248 6 stlink_usb.c:3746 stlink_open(): transport: 3 vid: 0x0483 pid: 0x3757 serial:
    Info : 249 19 stlink_usb.c:1475 stlink_usb_version(): STLINK V3J15M7B5S1 (API v3) VID:PID 0483:374F
    Debug: 250 19 stlink_usb.c:1696 stlink_usb_exit_mode(): MODE: 0x01
    Info : 251 19 stlink_usb.c:1507 stlink_usb_check_voltage(): Target voltage: 3.269841
    Debug: 252 19 stlink_usb.c:1764 stlink_usb_init_mode(): MODE: 0x01
    Debug: 253 19 stlink_usb.c:3130 stlink_dump_speed_map(): Supported clock speeds are:
    Debug: 254 19 stlink_usb.c:3133 stlink_dump_speed_map(): 21333 kHz
    Debug: 255 19 stlink_usb.c:3133 stlink_dump_speed_map(): 16000 kHz
    Debug: 256 19 stlink_usb.c:3133 stlink_dump_speed_map(): 12000 kHz
    Debug: 257 19 stlink_usb.c:3133 stlink_dump_speed_map(): 8000 kHz
    Debug: 258 19 stlink_usb.c:3133 stlink_dump_speed_map(): 1777 kHz
    Debug: 259 19 stlink_usb.c:3133 stlink_dump_speed_map(): 750 kHz
    Debug: 260 19 stlink_usb.c:1132 stlink_usb_error_check(): unknown/unexpected STLINK status code 0x5
    Error: 261 19 stlink_usb.c:3787 stlink_open(): init mode failed (unable to connect to the target)
    Debug: 262 19 stlink_usb.c:1696 stlink_usb_exit_mode(): MODE: 0x01
    Debug: 263 20 command.c:529 exec_command(): Command 'init' failed with error code -4
    User : 264 20 command.c:601 command_run_line():
    Debug: 265 20 breakpoints.c:328 breakpoint_remove_all_internal(): [STM32MP157CAAx.ap1] Delete all breakpoints
    Debug: 266 20 mem_ap.c:71 mem_ap_deinit_target(): mem_ap_deinit_target
    Debug: 267 20 target.c:2130 target_free_all_working_areas_restore(): freeing all working areas
    Debug: 268 20 breakpoints.c:328 breakpoint_remove_all_internal(): [STM32MP157CAAx.ap2] Delete all breakpoints
    Debug: 269 20 mem_ap.c:71 mem_ap_deinit_target(): mem_ap_deinit_target
    Debug: 270 20 target.c:2130 target_free_all_working_areas_restore(): freeing all working areas
    Debug: 271 20 breakpoints.c:328 breakpoint_remove_all_internal(): [STM32MP157CAAx.axi] Delete all breakpoints
    Debug: 272 20 mem_ap.c:71 mem_ap_deinit_target(): mem_ap_deinit_target
    Debug: 273 20 target.c:2130 target_free_all_working_areas_restore(): freeing all working areas
    Debug: 274 20 breakpoints.c:328 breakpoint_remove_all_internal(): [STM32MP157CAAx.cpu0] Delete all breakpoints
    Debug: 275 20 breakpoints.c:328 breakpoint_remove_all_internal(): [STM32MP157CAAx.cpu1] Delete all breakpoints
    Debug: 276 20 target.c:2130 target_free_all_working_areas_restore(): freeing all working areas
    Debug: 277 20 breakpoints.c:328 breakpoint_remove_all_internal(): [STM32MP157CAAx.cpu1] Delete all breakpoints
    Debug: 278 20 target.c:2130 target_free_all_working_areas_restore(): freeing all working areas
    Debug: 279 20 breakpoints.c:328 breakpoint_remove_all_internal(): [STM32MP157CAAx.cm4] Delete all breakpoints
    Debug: 280 20 target.c:2130 target_free_all_working_areas_restore(): freeing all working areas
    Debug: 281 21 arm_adi_v5.c:1217 dap_put_ap(): refcount AP#0x1 put 2
    Debug: 282 21 arm_adi_v5.c:1217 dap_put_ap(): refcount AP#0x1 put 1
    Debug: 283 21 arm_adi_v5.c:1217 dap_put_ap(): refcount AP#0x1 put 0
    Debug: 284 21 arm_adi_v5.c:1217 dap_put_ap(): refcount AP#0x2 put 0
    ST Employee
    November 5, 2024

    Hello @BuGe @UStei.1 and @DStau.1 ,

    Did you follow steps of the following Wiki page?

    If yes, could you please confirm that you had the same settings and are still unable to open a debug session?
    because I'm able to establish connection with CubeIDE 1.15.1 and latest image version available stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26 following the steps in the mentioned above Wiki page.

    STea_0-1730736686048.png

    Regards

    Visitor II
    November 12, 2024

    Hello STea,

    yes I know this Wiki of course and have the same settings. The only thing I changed was setting the interface from SWD to JTAG, because my baseboard provides only a parallel JTAG connector.

     

    Obviously, you changed the debug probe field from OpenOCD to GDB server. Doing that here, I get the following  log file attached (st-link_gdbserver_log.txt)

     

    On my Linux debug console, I can see the firmware booting:

    root@qsmp-1570:/home# [ 2156.292441] remoteproc remoteproc0: powering up m4
    [ 2156.302348] remoteproc remoteproc0: Booting fw image OpenAMP_TTY_echo_CM4.elf, size 2687680
    [ 2156.310558] rproc-virtio rproc-virtio.1.auto: assigned reserved memory node vdev0buffer@10042000
    [ 2156.320231] virtio_rpmsg_bus virtio0: rpmsg host is online
    [ 2156.325501] rproc-virtio rproc-virtio.1.auto: registered virtio0 (type 7)
    [ 2156.332357] remoteproc remoteproc0: remote processor m4 is now up
    [ 2156.338129] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty addr 0x400
    [ 2156.349738] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty addr 0x401

    also /dev/ttyRPMSG0/1 will be established.

    in the Reset behaviour field of the debugger settings I have choosen None.

    Is this correct? I wonder that the M4 firmware is obviously started, I would have expected that this is done by the debugger?