Debugging M4 with GDB from command line?
I would like to understand what the Eclipse IDE is doing to start the debugger, so that I can move away from using it. I much prefer CMake and other tools. I'd be grateful for any assistance. The wiki section for this is TBD.
I'm not too familiar with OpenOCD, but have run the command:
$OECORE_NATIVE_SYSROOT/usr/bin/openocd -s $OECORE_NATIVE_SYSROOT/usr/share/scripts -f board/stm32mp15x_dk2.cfg
This seems to work so, moving on to GDB:
$OECORE_NATIVE_SYSROOT/usr/bin/arm-openstlinux_weston-linux-gnueabi/arm-openstlinux_weston-linux-gnueabi-gdb firmware.elf
And this is where I come unstuck. I've used GDB a bit, but don't know the magic incantations to install an image into the M4 on this platform.
(gdb) target remote localhost:3333
Remote debugging using localhost:3333
0x00000000 in g_pfnVectors ()
I get a "target not yet examined" error which I don't understand. The vector table is all zeroes, so nothing has yet been placed in the RAM yet.
(gdb) load
Loading section .isr_vector, size 0x298 lma 0x0
Loading section .text, size 0x1688 lma 0x10000000
Load failed
Open On-Chip Debugger 0.10.0+dev-00546-g1afec4f-dirty (2019-02-01-13:33)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
debug_level: 1
cortex_a interrupt mask on
cortex_a interrupt mask on
cortex_a domain access control fixup on
cortex_a domain access control fixup on
3333
none separate
adapter speed: 5000 kHz
adapter_nsrst_assert_width: 200
adapter_nsrst_delay: 200
none srst_pulls_trst
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Error: Could not find MEM-AP to control the core
embedded:startup.tcl:24: Error:
in procedure 'stm32mp15x.cpu2'
in procedure 'ocd_bouncer'
at file "embedded:startup.tcl", line 24
undefined debug reason 7 - target needs reset
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
...