Question
Developer Package SDK Installation Failure
Hello!
I am having an issue installing the developer package SDK where the shell script is not found as well as an 'argument list too long' failure during setup.
I am using Ubuntu WSL to execute the script and see the following:
Any insight would be greatly appreciated!
sudo ./stm32mp1-openstlinux-5.4-dunfell-mp1-20-11-12/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1-openstlinux-5.4-dunfell-mp1-20-11-12.sh -d /mnt/c/Users/aortw/Documents/STM32MP15-Ecosystem/Developer-Package/SDK
./stm32mp1-openstlinux-5.4-dunfell-mp1-20-11-12/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1-openstlinux-5.4-dunfell-mp1-20-11-12.sh: 29: gcc: not found
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 3.1-openstlinux-5.4-dunfell-mp1-20-11-12
=======================================================================================================================
The directory "/mnt/c/Users/aortw/Documents/STM32MP15-Ecosystem/Developer-Package/SDK" already contains a SDK for this architecture.
If you continue, existing files will be overwritten! Proceed [y/N]? y
Extracting SDK....................................................................................................................................................................................................................done
Setting it up.../mnt/c/Users/aortw/Documents/STM32MP15-Ecosystem/Developer-Package/SDK/relocate_sdk.sh: 14: /usr/bin/python3: Argument list too long
SDK could not be set up. Relocate script failed. Abort!