Skip to main content
Visitor II
January 24, 2022
Question

Don't detects the board IP address. (Getting started STM32MP157x-DK2)

  • January 24, 2022
  • 1 reply
  • 1302 views

I'm trying develop on Cortex-M4 of "Getting started STM32MP157x-DK2".

I have a problem that don't detects the board IP address when "6 Check connection to the target" of Modify, rebuild and reload firmware.

However, Linux prompt are displayed in the console windows by clicking on the "STM32 butterfly button" and I can run Linux command on the board.

Serial target widget status icon is yellow light, and status is "idle".

I read STM32CubeIDE support wiki page (this page), but I can't discover solution this problem.

Are there any other settings that should be made?

Am I missing something?

I use STM32CubeIDE on Windows10 OS.

I'm not familiar English, so I'm sorry if my sentence is strange.

Best regards.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    February 1, 2022

    Hi @真çÂ�?†å­Â�? 石井​ ,

    How did you connect your board to ethernet .?

    With ethernet cable through a LAN ?

    With ethernet over USB using DK2 CN7 ?

    What gives "ifconfig" command on the target ?

    Are you able to ping the board ?

    Olivier