eMMC HS200 clarification
Hi there,
we are in the process of developing a product based on the STM32MP151F which will be USB powered (USB 2.0 device).
We are aiming to have it connected to an eMMC for mass storage and we would like to achive the highest R/W speed which should be 200MB/sec using HS200.
1) If my understanding is correct we cannot use the STM32MP157F-EV1 as starting point as the boards is using the STPMIC1A which regulates the eMMC VCCQ @3.3V and it incompatible with HS200, is it correct?
2) Has the STM32MP151 ever been tested at HS200 speed with a commercially available eMMC? Is there e refence design that e can use as starting point?
3) We have read the "2.3.19 DLYB limits SDMMC throughput" errata. Does it implies that HS200 is unusable? Or we can use it and it is just enough to disable the DLYB? If so why should we enable the DLYB in the first time?
4) If we use the STPMIC1B which regulates VDD at 1.8V making it compatible with HS200, is there any drop in the MPU performances?
5) Is there a reference design/app note covering the STM32MPU and STPMIC1 integration on an USB power supply? with 1.8V VDD possibly.
Thanks for your help,
Andrea