enable M4 log on STM32MP1 ( STM32MP157-DK2 dev kit)
Hello,
I am able to compile the M4 examples and it looks as though they run as expected ( I can see the log trace on the A7 side from the linux console). I would like to examine the log trace from the M4 side also as I would like to modify some of these examples for further use. In the OpenAMP_TTY_echo example (main.c) are the following lines
log_info("Cortex-M4 boot successful with STM32Cube FW version: v%ld.%ld.%ld \r\n",
((HAL_GetHalVersion() >> 24) & 0x000000FF),
((HAL_GetHalVersion() >> 16) & 0x000000FF),
((HAL_GetHalVersion() >> 8) & 0x000000FF));
I was curious as to how I can enable these lines. Do I need to enable putc associated with one of the UART instances or ..
Basically just want to know how I can have console functionality on the M4 side also
Thanks
Victor