Encountering Issues with Obtaining ADC Values via DMA
Hi All,
I have an question when i used STM32MP157.
I encountered an issue when using DMA to store the values of ADC conversions.
When I store the data from the ADC_DMA_Buffer to the ADC_DATA_Buffer in the HAL_ADC_ConvCpltCallback() function.
Then check the buffer values using STM32CubeIDE.
I notice that the ADC_DMA_Buffer[1] and ADC_DATA_Buffer[1], ADC_DATA_Buffer[3] ... do not match.
What could be the reason for this?
Here is the code and ADC1 configuration: (TIM2 frequency is 1000 Hz (1ms))
uint32_t ADC_DMA_Buffer[2] ={0};
uint32_t ADC_DATA_Buffer[500] ={0};
uint16_t ADC_Conversion_Done_Count = 0;
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
if(hadc->Instance == ADC1)
{
ADC_DATA_Buffer[ADC_Conversion_Done_Count] = ADC_DMA_Buffer[0];
ADC_Conversion_Done_Count++;
ADC_DATA_Buffer[ADC_Conversion_Done_Count] = ADC_DMA_Buffer[1];
ADC_Conversion_Done_Count++;
ADC_Conversion_Done_Count = ADC_Conversion_Done_Count % 500;
}
}
int main(void)
{
HAL_Init();
if(IS_ENGINEERING_BOOT_MODE())
{
SystemClock_Config();
}
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_ADC2_Init();
MX_TIM2_Init();
/* Run the ADC linear calibration in single-ended mode */
if (HAL_ADCEx_Calibration_Start(&hadc1,ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED) != HAL_OK)
{
Error_Handler();
}
if (HAL_ADCEx_Calibration_Start(&hadc2,ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED) != HAL_OK)
{
Error_Handler();
}
/* Start ADC conversion */
if (HAL_ADC_Start(&hadc2) != HAL_OK)
{
Error_Handler();
}
if (HAL_ADCEx_MultiModeStart_DMA(&hadc1, ADC_DMA_Buffer, 2) != HAL_OK)
{
Error_Handler();
}
/* Start Timer */
HAL_TIM_Base_Start(&htim2);
while (1)
{
}
}
static void MX_ADC1_Init(void)
{
ADC_MultiModeTypeDef multimode = {0};
ADC_ChannelConfTypeDef sConfig = {0};
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.NbrOfConversion = 2;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T2_TRGO;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc1.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure the ADC multi-mode
*/
multimode.Mode = ADC_DUALMODE_INTERL;
multimode.DualModeData = ADC_DUALMODEDATAFORMAT_DISABLED;
multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_5CYCLES;
if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel */
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
}
Best Regards,
Ken