Error in recipe st-image-resize-initrd while building openstlinux-5.4-dunfell-mp1-20-06-24
Hello,
I always get following error while building openstlinux-5.4-dunfell-mp1-20-06-24:
ERROR: st-image-resize-initrd-1.0-r0 do_rootfs: The postinstall intercept hook 'update_desktop_database' failed, details in /mnt/data/dist-pack/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs
ERROR: Logfile of failure stored in: /mnt/data/dist-pack/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs.3210
ERROR: Task (/mnt/data/dist-pack/openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb:do_rootfs) failed with exit code '1'Log file has this content:
[...]
NOTE: Running intercept scripts:
NOTE: > Executing update_desktop_database intercept ...
NOTE: Exit code 127. Output:
/mnt/data/dist-pack/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/intercept_scripts-485140355b6661d2198dd5380565982fade0f39d951f5e0daaeccda7f3a73ed0/update_desktop_database: line 7: update-desktop-database: command not found
ERROR: The postinstall intercept hook 'update_desktop_database' failed, details in /mnt/data/dist-pack/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/temp/log.do_rootfs
DEBUG: Python function do_rootfs finishedWhy is `update-desktop-database` command not found? How can I solve this?
Many thanks.
Kind regards!