facing ERROR: icu-66.1-r0 do_compile: oe_runmake failed during Building the OpenSTLinux distribution
Hi,
I'm working on STM32MP157A-DK1. By following this linkhttps://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package tried building the image for STM32MP157A-DK1 but i facing the error ERROR: icu-66.1-r0 do_compile: oe_runmake failed during build. attached build log.
i tried to resolve with the command "bitbake -c cleanall icu-native" and build still it fails. if i separately build "bitbake icu-native" it build fine but if i run command bitbake st-image-weston
the error comes up.