Failed to access ROM Table of CortexM4 while debugging in engineering mode. What are the reasons ? See description below.
Product: STM32MP153CAA3
we are trying to debug the Cortex M4 over the SWD Interface. The setup of the Bank0,1,2 is configured correct (Engineering Mode) . During the analysis of SWD we see that Debugger fails to access ROM Table (Address: 0xE00FFFE4, CM4ROM_PIDR1) Expected alue is 0x004. Read value is 0x7310F507
The IDCODE and the settings of registers before are matching the expectation.
What are the reasons for failing to access those registers ? (clocks, voltage ...)