Failed to start Load/Save Screen Backlight
Hi everyone,
I have encounter the following error when booting the stm32mp157f-dk2
Starting Load/Save Screen …of backlight:5a000000.dsi.0...
[FAILED] Failed to start Load/Save …s of backlight:5a000000.dsi.0.
See 'systemctl status systemd-backlight…ht:5a000000.dsi.0.service' for details.the 'systemctl status systemd-backlight@5a000000' give me the following
* systemd-backlight@5a000000.service - Load/Save Screen Backlight Brightness of
5a000000
Loaded: loaded (/lib/systemd/system/systemd-backlight@.service; static; vendor preset: disabled)
Active: inactive (dead)
Docs: man:systemd-backlight@.service(8)The screen is able to display the splash image during uboot, so I assume the hardware is OK. When calling a GUI application, it fail and report error as 'Could not initialize egl display'
Any ideas?