Skip to main content
Graduate
September 6, 2022
Question

Flash loop while populating the custom board with the V4.0.2 image

  • September 6, 2022
  • 0 replies
  • 732 views

Hi,

I have tried to migrate from ST Ecosystem 3.1 to 4.0.2 but I am unable to flash the image into the eMMC memory. My issue is similar to this one but I am using the Octavos SiP OSD32MP157c. As suggested by the original poster, the issue is probably the TF-A configuration.

The flash process is started but when the u-boot is supposed to be loaded the processor reboots and the process is repeated.

The image is created using device trees generated by STM32CubeMX 6.6.1 and I first generated the new trees and then copied changed parts from the generated trees for the DK2 board and my previous configuration.

For flashing I use STM32_Programmer_CLI and a micro-USB port. The flash log is attached below:

NOTICE: CPU: STM32MP157C?? Rev.Z
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
INFO: PMIC version = 0x21
INFO: Product_below_2v5=0: HSLVEN protected by HW
INFO: Reset reason (0x54):
INFO: System reset generated by MPU (MPSYSRST)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r1.0(debug):v2.6-dirty
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START...
INFO: phase ID :3, Manifestation 3 at c71186f3
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff226
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc5000
INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd9820
INFO: BL2: Skip loading image id 21
INFO: BL2: Skip loading image id 22
INFO: BL2: Loading image id 23
INFO: Loading image id=23 at address 0xc0500000
INFO: Image id=23 loaded: 0xc0500000 - 0xc0512d18
INFO: BL2: Loading image id 26
INFO: Loading image id=26 at address 0x2ffc0000
INFO: Image id=26 loaded: 0x2ffc0000 - 0x2ffc3ffd
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01ece98
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc5000
INFO: SPSR = 0x1d3
NOTICE: SP_MIN: v2.6-stm32mp1-r1.0(debug):v2.6-dirty
NOTICE: SP_MIN: Built : 13:14:26, Nov 23 2021
INFO: ARM GICv2 driver initialized
INFO: ETZPC: UART1 (3) could be non secure
INFO: ETZPC: SPI6 (4) could be non secure
INFO: ETZPC: I2C6 (12) could be non secure
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world
INFO: PSCI Power Domain Map:
INFO: Domain Node : Level 1, parent_node -1, State ON (0x0)
INFO: Domain Node : Level 0, parent_node 0, State ON (0x0)
INFO: CPU Node : MPID 0x0, parent_node 0, State ON (0x0)
INFO: CPU Node : MPID 0xffffffff, parent_node 0, State OFF (0x2)

Thanks for any suggestions.

Best regards,

Tomas

    This topic has been closed for replies.