Skip to main content
Visitor II
July 25, 2022
Question

gdbgui and STLink debug

  • July 25, 2022
  • 2 replies
  • 1631 views

From instructions, I opened two console:

Console 1: openocd -f board/stm32mp15x_dk2.cfg

This looks good as output:

 

```

...

Info : stm32mp15x.cm4: Cortex-M4 r0p1 processor detected

Info : stm32mp15x.cm4: target has 6 breakpoints, 4 watchpoints

Info : stm32mp15x.cpu0: hardware has 6 breakpoints, 4 watchpoints

Info : stm32mp15x.cpu0 rev 5, partnum c07, arch f, variant 0, implementor 41

Info : stm32mp15x.cpu0: MPIDR level2 0, cluster 0, core 0, multi core, no SMT

Info : stm32mp15x.cm4: external reset detected

Info : stm32mp15x.cpu1: hardware has 6 breakpoints, 4 watchpoints

Info : stm32mp15x.cpu1 rev 5, partnum c07, arch f, variant 0, implementor 41

Info : stm32mp15x.cpu1: MPIDR level2 0, cluster 0, core 1, multi core, no SMT

Info : gdb port disabled

Info : gdb port disabled

Info : gdb port disabled

Info : starting gdb server for stm32mp15x.cpu0 on 3333

Info : Listening on port 3333 for gdb connections

Info : starting gdb server for stm32mp15x.cm4 on 3334

Info : Listening on port 3334 for gdb connections

 

```

 

Console 2:

gdbgui -g "arm-ostl-linux-gnueabi-gdb -x gdb-script/Setup.gdb"

 

gdb-script folder is in same location where I run run command.

 

If I don't pass '-p 3333' then default is 127.0.0.1:5000 and failed.

If I add -p 3333 then:

 

OSError: [Errno 98] Address already in use

 

I already reset computer to "kill the gdbgui instance running in background" but did not help!

 

Anyone know how fix this issue?

 

And, the port is 5000 or 3333 if I want to debug over ST link?

 

edit:

Look to me port 3333 is right one. When look at console 1 where openocd start, I see:

 

```

Info : New GDB Connection: 1, Target stm32mp15x.cpu0, state: halted

Warn : ignoring character 0x47

Warn : ignoring character 0x45

.....

Warn : keep_alive() was not invoked in the 1000 ms timelimit. GDB alive packet not sent! (1016 ms). Workaround: increase "set remotetimeout" in GDB

```

 

When use port 5000 nothing happen at all.

Still see "OSError: [Errno 98] Address already in use" from gdbgui console if use port 3333

 

 

 

 

 

 

 

 

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    July 26, 2022

    Hi Dat Tran (Community Member),

    port 3333 is indeed the correct one to use

    Open On-Chip Debugger 0.11.0-rc2-dirty (2021-10-29-14:02)

    Licensed under GNU GPL v2

    For bug reports, read

    http://openocd.org/doc/doxygen/bugs.html

    srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst

    Info : Listening on port 6666 for tcl connections

    Info : Listening on port 4444 for telnet connections

    Info : STLINK V2J36M26 (API v2) VID:PID 0483:3752

    Info : Target voltage: 3.259064

    Info : Unable to match requested speed 5000 kHz, using 4000 kHz

    Info : Unable to match requested speed 5000 kHz, using 4000 kHz

    Info : clock speed 4000 kHz

    Info : stlink_dap_op_connect(connect)

    Info : SWD DPIDR 0x6ba02477

    Info : stlink_dap_op_connect(connect)

    Info : SWD DPIDR 0x6ba02477

    Info : stm32mp15x.cm4: hardware has 6 breakpoints, 4 watchpoints

    Info : stm32mp15x.cpu0: hardware has 6 breakpoints, 4 watchpoints

    Info : stm32mp15x.cpu1: hardware has 6 breakpoints, 4 watchpoints

    Info : stm32mp15x.cm4: external reset detected

    Info : starting gdb server for stm32mp15x.cpu0 on 3333

    Info : Listening on port 3333 for gdb connections

    Info : starting gdb server for stm32mp15x.cm4 on 3334

    Info : Listening on port 3334 for gdb connections

    Dat TranAuthor
    Visitor II
    July 26, 2022

    Yes, I will focus only on port 3333 from now.

    But when Openocd listen at port 3333

    And gdbgui also listen at port 3333,

    This causes another error: "Address already in use", and I read python source code, "SO_REUSEADDR" already set before bind socket.

    Do you have any idea?