GPIO SPI 5 miswired on STM32MP15 Discovery Kit MB1272
I was trying to use the GPIO expension connector on the STM32MP15 Discovery Kit MB1272 and the clock wasn't working on SPI5. When I checked the CubeMX configuration against the schematic for the discovery kit, I leaned that the clock signal is going to the Arduino connector instead of the GPIO expansion. The schematic insinuates that PF7 is SPI5_SCK, when it is actually PH6. Is this a known issue?