Hi,i am a beginner in MPU development. I have created cortex-M4 firmware project using stm32cubeide , but how can i start my firmware at the time of bootup?
i have read the article, https://wiki.st.com/stm32mpu/wiki/How_to_start_the_coprocessor_from_the_bootloader#Starting_the_coprocessor_firmware
where will i find this in my device tree
#define CONFIG_EXTRA_ENV_SETTINGS \
"stdin=serial\0" \
"stdout=serial\0" \
"stderr=serial\0" \
...
BOOTENV \
"m4fw_name=rproc-m4-fw.elf\0" \
"m4fw_addr=${kernel_addr_r}\0" \
"boot_m4fw=rproc init; rproc load 0 ${m4fw_addr} ${filesize}; rproc start 0\0" \
"boot_m4_mmc0=if ext4load mmc 0:4 ${m4fw_addr} ${m4fw_name} ; then run boot_m4fw; fi;\0"
"bootcmd=run boot_m4_mmc0; run bootcmd_mmc0\0"