How can i change the interface RGMII to RMII using CubeMX?
Hello Guys
Like the subject, I want change the interface RGMII to RMII using CubeMX.
(RealTek-RTL8211EG-VB-CG => Microchip - LAN8720AI-CP)
Based on STM32MP157C-EV1 Code in CubeMX, I changed the Ethernet option from RGMII to RMII as shown in the picture below.
And after Code Generating, I applied it to my addon(mx) directory and built it.
(Changed to the code generated by CubeMX.)
eth1_pins_mx: eth1_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_REF_CLK */
<STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
<STM32_PINMUX('G', 13, AF11)>, /* ETH1_TXD0 */
<STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
pins3 {
pinmux = <STM32_PINMUX('A', 7, AF11)>, /* ETH1_CRS_DV */
<STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
<STM32_PINMUX('C', 5, AF11)>; /* ETH1_RXD1 */
bias-disable;
};
pins4 {
pinmux = <STM32_PINMUX('B', 11, AF11)>; /* ETH1_TX_EN */
};
};
eth1_sleep_pins_mx: eth1_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 1, ANALOG)>, /* ETH1_REF_CLK */
<STM32_PINMUX('A', 2, ANALOG)>, /* ETH1_MDIO */
<STM32_PINMUX('A', 7, ANALOG)>, /* ETH1_CRS_DV */
<STM32_PINMUX('B', 11, ANALOG)>, /* ETH1_TX_EN */
<STM32_PINMUX('C', 1, ANALOG)>, /* ETH1_MDC */
<STM32_PINMUX('C', 4, ANALOG)>, /* ETH1_RXD0 */
<STM32_PINMUX('C', 5, ANALOG)>, /* ETH1_RXD1 */
<STM32_PINMUX('G', 13, ANALOG)>, /* ETH1_TXD0 */
<STM32_PINMUX('G', 14, ANALOG)>; /* ETH1_TXD1 */
};
};
ðernet0{
pinctrl-names = "default", "sleep";
pinctrl-0 = <ð1_pins_mx>;
pinctrl-1 = <ð1_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN ethernet0 */
phy-mode = "rgmii-id";
/*phy-mode = "rmii";*/
max-speed = <1000>;
phy-handle = <&phy0>;
mdio0{
#address-cells = <1>;
#size-cells = <0>;
compatible = "snps,dwmac-mdio";
phy0:ethernet-phy@0{
reg = <0>;
};
};
/* USER CODE END ethernet0 */
};However, it seems that the ethernet chip is not recognized as shown in the log below.
~# dmesg | grep eth
[ 0.000000] psci: probing for conduit method from DT.
[ 1.236408] usbcore: registered new interface driver cdc_ether
[ 2.756520] stm32-dwmac 5800a000.ethernet: PTP uses main clock
[ 2.760976] stm32-dwmac 5800a000.ethernet: no reset control found
[ 2.767028] stm32-dwmac 5800a000.ethernet: No phy clock provided...
[ 2.773905] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42
[ 2.780299] stm32-dwmac 5800a000.ethernet: DWMAC4/5
[ 2.785190] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported
[ 2.792527] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported
[ 2.799835] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported
[ 2.806696] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported
[ 2.812984] stm32-dwmac 5800a000.ethernet: TSO supported
[ 2.818278] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 2.826149] stm32-dwmac 5800a000.ethernet: device MAC address be:10:95:ec:a0:c7
[ 2.833449] stm32-dwmac 5800a000.ethernet: TSO feature enabled
[ 10.455282] stm32-dwmac 5800a000.ethernet eth0: no phy at addr -1
[ 10.475335] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Cannot attach to PHY (error: -19)I have no experience changing ethernet ICs so I need your help.
If necessary, I can attach the ethernet circuit diagram of my board.
Thanks