how can i flash a data with STM32PRogrammer into gp0 partition of eMMC
Hallo everybody,
I have a problem with flashing a data into GP0 partition of eMMC. I have added 2 General Purpose Partitions to our eMMC and left 32MB free userspace. Now a STM32Programmer can see only a 32MB of the userspace and i can not flash an image into GP-Partition. STM32Programmer say: mmc0 max address is 0x1f80000 and mmc1 and mmc2 are not available. Are there some special options to recognize another 2 GP-Partitions I added with linux mmc-tool?
Thanks in advance.