Skip to main content
Visitor II
April 22, 2022
Question

How can I load a MAC address from EEPROM on an ST32MP157f at boot time using the device tree?

  • April 22, 2022
  • 1 reply
  • 1154 views

 I can read the eeprom in uboot and the kernel. If I add

ethernet@...{ 

local-mac-address = [ 00 01 02 030 40 05];

};

to the device tree it will be used by the kernel. I can't seem to get any other device tree modifications to work. I'm using a stock kernel, and I'm not sure what other information might be relevant. That you for your attention.

-russ

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    June 9, 2022

    Hello @Russ​ ,

    Sorry for the delay.

    I think the major problem with this setup is that you must be sure that I2C (that handles EEPROM) is initialized before the ethernet.

    Do you still need help on this topic?

    Regards,

    Kevin

    Russ1Author
    Visitor II
    June 9, 2022
    As it turns out, yes, I still need assistance with this. I imagine I have a device tree entry wrong, but I have been working on other STM32MP1 audio tasks related to a certain firm in Australia. Can you point me to a document or app note that describes this? I’m using a stock 5.18.0 kernel and have been able to get most everything else I need functioning.

    Thanks for your assistance…

    -russ